MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can not get data interrupts or data generation working properly

We are so frustrated right now, we have spent days reading the data sheets, which has many errors, and the app note 3308 which is random and sketchy at best, but we are stuck with this part on a production design and need to implement the most basic ...

Herb by Associate
  • 809 Views
  • 0 replies
  • 0 kudos

Unicleo - Comms protocol? Source code?

Is the comms protocol between the Unicleo GUI PC application and the Nucleo board documented anywhere?If so, where?The Unicleo GUI is touted as part of the "Open Development Environment", but I can't see any source code anywhere.Is it published?If so...

CubeMX + X-CUBE-MEMS1 application generation for a "custom" board. Is there a way to replace the word custom when generating the code?

The generated code may contain hundreds of occurrences of custom*, CUSTOM* and some custom file+folder names. Renaming this afterwards is cumbersome, even when using tools. Moreover, this has to be done after each code re-generation. Are there means ...

KnarfB by Super User
  • 1071 Views
  • 0 replies
  • 0 kudos

BLE_SensorDemo increase audio GATT Char value MTU size

I have an STM Blue Tile and I want to send the data picked up by the microphone over BLE at a rate of 16KByte/second without using the Codec. The out of box code in BLE_SensorDemo seems to pick up the audio using MEMS microphone at a rate of 8KByte/s...

PRiva by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

BlueNRG aci_gatt_update_char_value() api failing to send notifications due to large Delay before receiving Tx Pool Available Event

Hello,I am using ST-Sensortile dev kit and BlueNRG stack. I have to achieve @100Hz rate sending notification from sensortile to cell phone app based BLE central. I am using aci_gatt_update_char_value() api to send notification for live streaming of a...

IGaub by Associate
  • 878 Views
  • 0 replies
  • 0 kudos

Resolved! Different sensors with same name LSM6DS0 ????

Currently I'm working with an "old" IKS01A1 expansion board which should be populated with a LSM6DSO 3D acceleration and gyroscope sensor:But running the X-CUBE-MEMS1 software fails due to a wrong chip ID.The software expects 0x6C but the chip has 0x...

0690X00000A9S6jQAF.png 0690X00000A9S6UQAV.png 0690X00000A9S6yQAF.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.