2019-08-14 3:50 AM
Hello, ST community!
Recently I got a custom board from my customer to help with creating the lsm303agr driver.
What I'm struggling with is the temperature sensor reading. No matter what I do, the sensor returns 0x0 0x81
Here is a dump from lsm303agr ACC registers prior to reading sensor data.
# Log format: [%register_address%] -> %register_value%
acc: [0x7] -> 0xff
acc: [0xf] -> 0x33
acc: [0x1f] -> 0xc0
acc: [0x20] -> 0x47
acc: [0x21] -> 0x0
acc: [0x22] -> 0x0
acc: [0x23] -> 0x90
acc: [0x24] -> 0x0
acc: [0x25] -> 0x0
acc: [0x27] -> 0xff
acc: [0x3e] -> 0x0
acc: [0x3f] -> 0x0
acc: [0x25] -> 0x0So three requirements are met, according to log:
Here is a code of getting sensor data (for clarity):
while (1) {
delay_ms(1000);
uint8_t buf[6];
/* Burst read function: 1 argument is a device,
* second is a register address, 3rd and 4th - buffer and its size
*/
lsm303agr_burst_read(SELECTOR_ACC, 0x0C, buf, 2);
printf("--> %#x %#x\r\n", buf[0], buf[1]);
/* For convinience, I'm also printing ACC data */
lsm303agr_burst_read(SELECTOR_ACC, REG_OUT_X_L_A, buf, 6);
printf("--> %#x %#x; %#x %#x; %#x %#x\r\n", buf[0], buf[1], buf[2], buf[3], buf[4], buf[5]);
}This is the output of that code:
--> 0x0 0x81
--> 0x80 0xff; 0x0 0xff; 0xc0 0x1e
--> 0x0 0x81
--> 0xc0 0xff; 0xc0 0xfe; 0xc0 0x1f
--> 0x0 0x81
--> 0x40 0x0; 0x80 0xfe; 0xc0 0x1e
--> 0x0 0x81
--> 0x0 0x0; 0x0 0xff; 0x80 0x1e
# ...and so onAs you may see, accelerometer data is read correctly, but temperature - isn't.
Could you please guide me what might be wrong here?
Regards,
Max
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.