MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How should data ready output be configured for LIS2MDL.

I've tried to use LIS2MDL with interrupts without success.What needs to be done, and does it work with continuous mode?It looks (by the data sheet) like enabling the DRDY (bit 0 in CFG_REG_C) would be enough, but seems not.It looks like DRDY is not a...

SensorTile.box #3: A small, portable weather station

The first example application we see is the Barometer. It's on of the simplest applications because it consists only of Inputs (the Sensors) and one Output (stream to BLE). No operations (called in this case "functions") are performed on the data in ...

0690X000009jGhlQAE.png

HTS221 temperature stuck at 35C and unreliable humidity measurement

Hi there,I managed to solder about 20 HTS221 on my custom board using a small oven, some boards have a correct temperature and humidity measurement, but others are out of luck.issue 1:temperature stuck around 35C, in my room at 24c, changes on the te...

0690X000009jKQeQAM.png
JISEA by Associate
  • 1454 Views
  • 1 replies
  • 0 kudos

LIS3DH drift over time

HelloI was asked to build a device which will determine if a box is in either of the three following states: perpendicular to ground, tilted forwards (10° or more), tilted backwards (10° or more). I am attaching a simple drawing for visualization of ...

LIS3DSH SPI address increment problem

I am using an ST Micro MCU via SPI to the LIS3DSH to read x,y,z data(using CubeMX HAL). I can read in single byte mode fine but the multi byte access bit in Control register 6 has no effect. I have tried Control register 6 : ADD_INC disabled or enab...

PVall by Associate II
  • 1288 Views
  • 2 replies
  • 0 kudos

LSM6DSM loses its configuration.

LSM6DSM loses its configuration when another chip in the board is turned on. SIMO pin goes up for 1.5ms when it happens, with a voltage of 2.2V even though the accelerometer is fed with a 2.8V supply voltage. I do not see a glitch below 1.8V which co...

SRezk by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.