MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS33HW accuracy question

Hello,I have a question related to accuracy of this sensor see attachmentFrom the datasheet I can read that the accuracy over temperature is +/2.5hPa. Did I correctly understand that the accuracy of the sensor can change within this range only in thi...

I am working on using an STM32L4 as a SMBus host to communicate to a battery monitor IC with many different registers. Using cubeMX and HAL to generate my code, I am having trouble understanding the functions and variables. Help!

From what I understand, the slave device I want to communicate with has many addressed registers than I need to specify in addition to the slave device's address. If the slave device's address is 0x16, and the registers I need to read on that device ...

JLand.8 by Associate
  • 1032 Views
  • 0 replies
  • 0 kudos

SensorTile.box #6: Why should I use the ST.box Expert mode

Why should one need something more, if a lot of everyday-life applications are already available by default as examples? Different reasons, indeed:Power optimization: Individual sensors can be activated or shut down to enable only the required sensor...

IIS2MDCTR temperature rating.

Please present the junction temperature rating of IIS2MDCTR,Is it generally the same as the storage temperature?

HTaka.8 by Associate
  • 1198 Views
  • 1 replies
  • 0 kudos

Resolved! LSM9DS1 Temperature

HI,I've problems on the temperature detected by the LSM9DS1. I used the "Unico" software to configure the Acc/Gyro and the Magnetometer, in particular I used the "Easy configuration button".I read the temperature (Unico page Acc/Gyro Registers) from ...

HTS221 water resistance

The HTS221 can handle condensation, according to the data sheet.According to that, I understand that water will not damage the sensor.(I refer to the sensing area on top, to the contacts on the bottom.)Is this correct?

GShim by Associate II
  • 1737 Views
  • 4 replies
  • 0 kudos

Configuration of MKI109V3, Unico, and MKI197V1

I am attempting to evaluate the LSM6DSOX IMU using the combination of MKI109V3, MKI971V1, and Unico.This is the same combination shown in several of ST's YouTube videosAll of the products are new and have not previously been installed or used.I have ...

0690X000009juuLQAQ.png 0690X000009juuQQAQ.png 0690X000009juv9QAA.png
ARenn.12 by Associate
  • 1116 Views
  • 2 replies
  • 1 kudos

SensorTile.box #5: From Entry-level to Expert mode

Till now, the described application are already-packed apps that can be simply downloaded on the Sensortile.box with just a click. Expert mode allows you to create your own application/algorithm by using Expert View in ST BLE Sensor application. We ...

0690X000009jxDAQAY.png

Resolved! LSM303AGR return only zeros

It's returning ack on the i2c on every command , and i'm getting an error if it's not the correct address.I'm attaching image from the scope of the i2c commands and responses.The configuration done first and then I'm reading the temperature that it a...

netanelu by Associate III
  • 3782 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.