2019-09-29 9:05 PM
Please present the junction temperature rating of IIS2MDCTR,
Is it generally the same as the storage temperature?
2019-10-04 6:17 AM
Hi @HTaka.8 , please check if I well interpreted you question. The IIS2MDCTR max supply is 3.6V and max current (high performance mode, max ODR) is 1130uA, so the power consumed in the worst case is P=V*I=4mW. If you consider that the device package thermal resistance is 80°C/W, the thermal difference between the device and the environment is DeltaT=0.3°C worst case. Moreover, no worry about the junction temperature with respect to storage temperature. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.