Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
I looked into the user manual, but don't really know how to calculate that. I'd really appreciate it if someone could give me some clue on that
i use the lis2dh12 accelerometer and lis3mdl magnetometer for making tilt compensated compass. i read datasheet and application but i have below list of confusionq 1] which type of data of accelerometer is used for calulate roll and pitch either...
When leaving pins 2 and 3 of the LSM6DSM unconnected, the device's consumption can increase over time and eventually reach 400 uA. Why is that? could you provide a block diagram of the device?
LSM6DSM pull up configuration for pins 2 and 3 is not working in Mode 1. Does it require something else, besides setting the flag PULL_UP_EN in 1?
Hello,I'm having problems with free fall interrupt. I set every register that needed to be set with values that are written in application note of sensor.57h to CTRL_REG100h to CTRL_REG240h to CTRL_REG300h to CTRL_REG408h to CTRL_REG516h to INT1_THS0...
Hi, Could anyone to explain the meaning of "3200" number in Table 10. Operating modes - low-noise setting disabled (LIS2DW12 Datasheet).Is it Bandwidth in Hz?What is practical meaning of it if max ODR is resricted to 200 Hz only?BR, Oleg
I am extracting LSM6DSL's data at FIFO rate 833 Hz and I set the SPI rate at 10MHz which is the max rate that the IMU can tolerant,I thought it should be fast enough for 833 Hz FIFO rate? See the picture below (( plz Ignore the title in the picture i...
Our application requires extraction of angle from the gyro samples over short periods of time- a few seconds. In other words, we need to integrate the gyros. We see that when we integrate the data when the device is static the accumulated error is fi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.