2019-10-30 7:57 AM
Hello,
I'm having problems with free fall interrupt. I set every register that needed to be set with values that are written in application note of sensor.
57h to CTRL_REG1
00h to CTRL_REG2
40h to CTRL_REG3
00h to CTRL_REG4
08h to CTRL_REG5
16h to INT1_THS
03h to INT1_DURATION
95h to INT1_CFG
Read INT1_SRC after interrupt happens.
I'm using NUCLEO F091RC where i'm detecting external interrupts on INT1 pin.
I think it happened once that interrupt was triggered but that's it or maybe pull-down resistors weren't set at that time.
I really don't have any idea what's wrong. DRDY signal on INT1 doesnt work either and was set like FF interrupt from application note.
I would really appriciate help from you.
2019-11-04 8:57 AM
Hi @TM.634 , on which pin of the NUCLEO F091RC board did you wired the INT1 pin of the LIS3DH? Did you check if it is not a reserved line (also with an oscilloscope)? Supposing everything is ok from an HW p.o.v., can you please confirm me you are reading sensible data and no issue on I2C/SPI communication? One test you could do is to increase or decrease the free fall threshold (actually 16h = 350mg in INT1_THS). Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.