MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X problem connecting to Nucleo F401RE

HiI have been working with the Nucleo F401RE + P-NUCLEO-53L0A1 sampling the VL53L0X, and it was working fine. However interfacing the Nucleo F401RE  to another VL53L0X module (https://picclick.de/VL53L0X-Time-of-Flight-Distance-Sensor-Breakout-GY-VL5...

Aharon1 by Associate II
  • 1232 Views
  • 0 replies
  • 0 kudos

Using DHT22(AM2302) sensor

Hi,I'm looking for some example how to use the sensor with STM32 and wonder why all of them, which I've found, are based on the loop not on interrupts.The response is 40 bits and it takes up to several milliseconds to read it, so during the time MCU ...

not getting accelerator axis values

Hi.We have a board based on nordik nrf52840 chip with lis3dh accelerator sensor connected.i took the driver code for lis3dh from STM github and wrote the context functions using nordic sdk 15.2 (I2C bus). First of all i must say that the ADDRESS in ...

eyal.gal by Associate II
  • 4831 Views
  • 8 replies
  • 0 kudos

LSM6DSOX SPI ack

Hi,I am using an LSM6DSOX in SPI mode. I prefer SPI over I2C because it has bigger data transfer rates. Is there any way to be sure that my SPI commands were executed with success? Are they returning something? For example, how can I be sure of the i...

UM2116, on p. 16

 In the document titled "STEVAL-MKI109V3 Professional MEMS Tool motherboard for MEMS adapter boards" UM2116, on p. 16 it is listed that the returned value from the *start command is: s t A_XH A_XL A_YH A_YL A_ZH A_ZL Int1 Int2 TL TH sw1|sw2 \r \n . T...

EHD by Associate II
  • 745 Views
  • 0 replies
  • 0 kudos

Resolved! IIS2MDC single measurement current consumption

Hi,We notice IIS2MDC have single measurement mode which can be used for one shot operation. The datasheet also mention how to calculate current consumption for such mode.However we can not find if the sensor will go sleep immediately after measuremen...

Dillah by Associate II
  • 1530 Views
  • 1 replies
  • 0 kudos

Resolved! Is the ODR of LSM6DS3 the same as sampling frequency?

Hello, I want to use a accelerometer which is LSM6DS3, and it's spec says that it's maximum ODR is 6600Hz.So I want to know is the ODR the same as sampling frequency?Or is it just out data rate? And is sampling frequency less than ODR? If so, what's...

Ray Sun by Associate
  • 1431 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.