MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to handle e-Compass thermal drift

We do some initial validation of LIS3MDL and experienced a problem when we do a temperature cycle (20°C to 80°C in 20 minutes) in an oven with 7 sensors inside and no external magnetic field present.It seems that we get an offset in the output signal...

SensorTile.box USB connection does not work.

I am trying to work through the labs from the recent ST sensors workshop. The very first step in the Pro-mode lab is to enter the DFU mode and program the SensorTile.box with a precompiled image. The problem is that when I connect the tile to my co...

Rita Ch. by Associate II
  • 3143 Views
  • 4 replies
  • 0 kudos

LSM9DS1 BDU Details

Hi everyone,Does the block data update mode block also the sensor's sampling? Or simply the sensor continues to acquire and the registers are just not updated until the next reading? It's very important to me because I use LSM9DS1 gyroscope and accel...

Burst Reading the LSM6DSM FIFO

I am reading the LSM6DSM FIFO with the accel and gyro enabled. I burst read 12 bytes using the SPI. One output byte to say to read the fifo then 12 input bytes (6 bytes of accel and 6 bytes of gyro). That works great. I tried reading more than 12 byt...

Can't vary duration on LIS3DH fall detection

I have been trying to setup fall detection interrupt on LIS3DH. I can get it to work but only with specific setup. In particular INT1_DURATION values: 0x05 works (but is too short) so my global setup is ok. But with any other duration values, even ju...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.