2019-12-09 6:43 AM
For example, given the following data taken from the sensor should the Y reading marked with a * account for a buffer overflow and therefore the difference be calculated as follows: 0xffff - 0xffd4 + 0x0e88 = 0x0eb3
Initial X Reading: 0x0068
Self-Test X Reading: 0x10c0
Delta: 0x1058
Initial Y Reading: 0xffd4
Self-Test Y Reading: 0x0e88
Delta: 0xf14c *
Initial Z Reading: 0xb00c
Self-Test Z Reading: 0xed68
Delta: 0x3d5c
2019-12-16 7:52 AM
Hi @AJohn.2439 , did you refer to p.43 of AN5038 for the Self-test procedure? And did you take into account the two recommendations of waiting for 100ms for stable output and to discard the first sample read after the sensor has been turned on? Waiting for output stability (and a stable environment indeed) is as well important in the self test performance. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.