VL53L1 supply voltage.
Is It safe to power VL53L1 by 3.3v for continuous operation?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Is It safe to power VL53L1 by 3.3v for continuous operation?
STMicroelectronics is pleased to invite you to the Interactive Cross Fertilization Day.The event will take place on February 4th, 2020 at our site in Cornaredo, Via Monzoro 180 (Palazzo Quadrifoglio) starting from 9:30.More details in the attached fi...
I have a system containing a LSM9DS1 sampling AXL and Mag at 50Hz (gyro is disabled). When the LSM9DS1 is not attached (desoldered) our system (MCU only) draws about 2mA (10mV average over a 5 ohm resistor). This is constant and stable current of 2mA...
I am using the LSM9DS1 in our application with no problems normally. The gyro, axl and mag sensor all operating as requied. All written settings e.g. +/- range are set ok, and all registers read are giving the right outputs as device is moved around ...
Hi,I'm trying to simply read WHO_AM_I (0Fh). OUT_Z_L (2Ch) and OUT_Z_H (2Dh) registers. But output data is only FFh. Also other registers too. What is the data sequence for simple read function? My SPI bus output is MSB first and clock idles low. Fo...
I am using the code provided in the TN1218 sheet, and I've attached a screenshot of my variables.
We have a design with LPS35HW where the part sometimes doesn't respond on the SPI bus at startup. A power cycle clears the issue. Any ideas on what could cause this?
are LSM6DSOX+IIS2MDCTR a good match for a sensorfusion setup, where we want absolute heading as quaternions?should the ISS2 be connected to the slave port of LSM6?regards,Henrik
are LSM6DSOX+IIS2MDCTR a good match for a sensorfusion setup, where we want absolute heading as quaternions?should the ISS2 be connected to the slave port of LSM6?regards,Henrik
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.