MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Motionfx library on any stm32?

Hello,I have a nucleo and a expansion board and i use it to get raw data from accelerometer,magnetometer and gyroscope.My question is How I use the motionfx library? Can I get for example quaternions? I can 't find any source code for motionfx!

suads by Associate III
  • 3048 Views
  • 6 replies
  • 0 kudos

How to get started with E-compass library for the Sensortile.Box?

Hello All,I have been planning on a project around the sensortile box. For this project I wanted to use multiple sensortile box modules and have each of them send their heading directions via bluetooth to a master PC or a HUB.I am aware of the FP-SNS...

VRao.1 by Associate III
  • 1147 Views
  • 1 replies
  • 0 kudos

How does the FIFO works for LSM6DSO

Hi,I was wandering how the FIFO works in terms of reading and writing data at the same time. While I am reading the FIFO, what happens with the new data that is generated from the accelerometer? Am I losing this data, or is it stored in the FIFO agai...

Accuracy of IIS3DHHC

IIS3DHHC When used as an inclinometer, what is the minimum angular resolution?Posted on June 08, 2018 at 23:30The IIS3DHHC is a triaxial accelerometer that outputs 16-bit data, 3-axis, �2.5 g acceleration data.So (5g)/(2^16 bits) = 7.63*10^-5 g's/LSB...

htamas by Associate
  • 1098 Views
  • 1 replies
  • 0 kudos

Auto-wakeup from low-power mode(standby mode) for STwinkT

from this video in another product, i did understand how to make the stm32 product go to standy. But how do i do the auto wakeup from low power mode. I saw from the reference Manual for stm32l4 To wakeup from Standby mode, there is no need to configu...

reokyouma by Associate III
  • 919 Views
  • 1 replies
  • 0 kudos

What is the difference between LIS2DH and MIS2DH?

Hi.​Currently I'm using LIS2DH12, and I found a new product, MIS2DH.​Actually, we are developing a medical device, and it seems that MIS2DH is a accelerometer devloped for medical applications.​But I cannot find any difference between two sensors.​Is...

wonhyuck by Associate
  • 1024 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.