2020-03-20 10:47 AM
Hi everyone,
I'm using the quaternions and the sensor fusion in Algobuilder with the Sensortile box in order to compare the signal of the quaternions and the position of the teapot, but I don't understand the relation between both of them... Any idea?
When I turn the Sensortile box 90° in X-axis, the teapot turns -90°.... WHY???
Thanks!
2020-03-20 12:37 PM
"Conpare the signal of the quaternions And the position of the teapot"
When did Lewis Carroll start writing code?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.