MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303AH SPI FIFO burst read producing zeros

Hi, I am working with the LSM303AH (accelerometer + magnetometer) as a potential replacement to the LIS2DS12 (accelerometer only). The accelerometer section of both devices seems identical with the only exception being the SPI on the LSM303AH is 3 wi...

Resolved! How to decode LIS2DU12 QR code marking

We have purchased some LIS2DU12 and when scanning the QR code markings we see 78327KT603ES0YJ on some and 78327KT603EO0YZ on others. What is the difference? And how do we decode the QR code, didn't see anything on the datasheet?Thanks.

Lazaro by Associate II
  • 2198 Views
  • 5 replies
  • 0 kudos

Resolved! IIS2DLPC Bandwidth

Hi ,I see that the bandwidth of IIS2DLPC is 3200 Hz for low power mode 1 according to the datasheet (page 22 ). Also it mentions that the maximum ODR is 200 Hz for this mode. This looks contradictory to me as 3200Hz bandwidth won't be compatible with...

KJose.1 by Associate III
  • 1244 Views
  • 3 replies
  • 2 kudos

AIS2IH Register issue

I'm working with the AIS2IH accelerometer.  I've established communication via SPI, and am able to read the WHOAMI correctly, along with requesting and receiving data as expected.  However, some of the data I'm reading doesn't make a lot of sense, so...

icachr by Associate
  • 703 Views
  • 2 replies
  • 0 kudos

Resolved! IIS2DULPX one shot setup

Hello I suspect I'm about to make a dumb question but I've been strugling for the past 2 days trying to just make a simple reading of the accelerometer. Just that get those values out of X, Y and Z axis...I can get the correct responses out of the WH...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.