2025-05-15 1:09 AM - edited 2025-05-15 1:10 AM
Hi,
my company is currently evaluating usage of the IIS2DULPX accelerometer in one of the products we are developing. Our use case requires that a wake-up interrupt is generated whenever acceleration sample exceeds a set threshold value. However, we would like to generate this interrupt with a threshold that takes into account either:
We would like to do so while keeping the ODR at 400-800 Hz and the ability to configure threshold as a value in a full +/- 16g range.
From the data sheet it seems that the wake-up feature is fed by an internal slope filter, making it impossible to use wake-up feature as I have specified above. Therefore, is it possible to either disable the slope filter or achieve the aforementioned functionality with use of one of the advanced features, such as finite state machine or machine learning core modules?
Kind regards,
Robert
Solved! Go to Solution.
2025-06-04 7:36 AM
Hi @td-robhyn ,
I confirm that wake up is not suitable for your case, but you can make your own MLC or FSM algorithm, keep in mind, however, that each device has its own offset, each of them will have to be configured with FSM and/or MLC that take into account its specific offset.
2025-06-04 7:36 AM
Hi @td-robhyn ,
I confirm that wake up is not suitable for your case, but you can make your own MLC or FSM algorithm, keep in mind, however, that each device has its own offset, each of them will have to be configured with FSM and/or MLC that take into account its specific offset.
2025-06-06 6:05 AM
Hi @Federica Bossi,
thank you for your reply. Indeed, we have managed to create an FSM algorithm that would work and evaluated it on the MKI109D eval-board. Unfortunately though, it turned out that the power consumption of the sensor with FSM enabled and running at 400 Hz is too high for our use case (>32 uA at 1.8V).
Kind regards,
Robert
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.