MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about the sign of raw sensor measurement

I have a problem when i read the AN4508 application notes.In the figure shown below, Xb, Yb and Zb are device body axes with a forward-right-down configuration. XA, YA and ZA are the accelerometer sensing axes.When sensor is placed still on the table...

0693W000001sakMQAQ.png 0693W000001sakvQAA.jpg 0693W000001salAQAQ.png
llau.1 by Associate
  • 1335 Views
  • 1 replies
  • 0 kudos

Resolved! LIS331DLH chips I got show wrong value under low temperature.

hello. I have a question about LIS331DLH. ​under low temperature, LIS331DLH chip z-axis shows wrong value.it is almost 100 difference between -10 degree and 22 degree. x,y axis is fine but only z axis is problem. every chip I got have same problem ex...

kdok .1 by Associate II
  • 1582 Views
  • 2 replies
  • 0 kudos

VL53L0X long range mode

I am using VL53l0x and I want to measure distances of 2 meters but I don't find the function to configure long range mode.

Mcabe.1 by Associate II
  • 783 Views
  • 0 replies
  • 0 kudos

Set LIS2DH12 in power down mode

Hello ST Community,My application involves nRF52 series processor which interfaces with LIS2DH12 via SPI and I am trying to reduce the power consumption as much as possible when the processor is in sleep mode. I understand that, as soon as power is a...

AB.4 by Associate II
  • 2159 Views
  • 2 replies
  • 0 kudos

Algobuilder IIR Filter a10/a20 coefficient

Hi!I am using the IIR function block in Algobuilder. In the UI I can enter the coefficients manually or use a file. The implementation uses the CMSIS functions Biquad Cascade IIR Filters Using Direct Form I Structure (void arm_biquad_cascade_df1_init...

DWind.1 by Associate III
  • 1349 Views
  • 1 replies
  • 0 kudos

Export raw accelerometer- and FFT-values from Unicleo

Hi!I have a Nucleo board and use the FFT example that comes with Algobuilder. It shows all the data and the results from FFT in the separate window. I would like to export all the data (accelerometer values, FFT results, peaks, etc). It works with ac...

0693W000001scykQAA.jpg
DWind.1 by Associate III
  • 1028 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.