MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DH12 zero-g level offset.

Hello everyone,I'm using lis2dh12 for acceleration measurement. In the datasheet, I find the typical zero-g offset accuracy is +/-40mg. When the device is placed horizontally, the reading of X-axis and Y-axis should be 0. For most of our devices, the...

lbing.1 by Associate II
  • 1612 Views
  • 2 replies
  • 0 kudos

LIS3DH accelorometer based on i2c

Hi,we are woeking on motion detection application using LIS3DH,we have done below registersettings but we are only getting interrupt on motion first time but after that we are not getting interrupt after reset also.once we are getting th einterrupt a...

AKUMA.1 by Associate
  • 1414 Views
  • 2 replies
  • 0 kudos

ERROR MESSAGE

HI everyone, I have this error message when I compile my main program with eclipse ... I'm using a P Nucleo 53L0A1 .. someone can tell me what's happening because I really don't understanderror message =>Open On-Chip Debugger 0.10.0+dev-00021-g524e8c...

MSAMB.1 by Associate III
  • 991 Views
  • 1 replies
  • 0 kudos

LPS22HB address?

Hi.I'm testing pressure using LPS22HB IC.I connect GND SD0.But LPS22HB give me address nack.So I change address "Low" to "High", LPS22HB give me strange pressure value and not address nack.Why do LPS22HB address strange?Thank you.

JLee.21 by Associate II
  • 3632 Views
  • 6 replies
  • 0 kudos

What is modulus of acceleration?

In Design Tip DT0106, is it mentioned that:Another technique which can be of help in controlling the integration error is known as Zero-Velocity-Update (ZVU): when the modulus of the acceleration is 1g and the output of the gyroscope is near 0, then ...

NLe.1 by Associate
  • 2084 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.