MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB non-volatile calibration ?

I'm currently using the LPS22HB pressure sensor in order to make a CO2 sensor more accurate. We need to calibrate the pressure sensor so it doesn't incorrectly modify the CO2 reading. We are having difficulty understanding wether the one point calibr...

JDart.1 by Associate
  • 1331 Views
  • 1 replies
  • 0 kudos

How to collect sensor fusion and IMU sensor data csv data concurrently on the ST BLE Sensor App with the Steval-STLKT01V1?

On the ST BLE Sensor App, I can only able to either export Accelerometer, Gyroscope, and Magnetometer csv files OR Sensor Fusion csv file. I was wondering if there is a way to export both of these files? Another question, I was wondering if there is ...

NLe.1 by Associate
  • 1242 Views
  • 1 replies
  • 0 kudos

Resolved! steval-mki181v1 - i2c connected problem...

Hi, im have:https://www.st.com/en/evaluation-tools/steval-mki181v1.htmlI have connected after i2c in esp32. It works and sometimes disconnects it. Do you need to use any resistors?

TBart.1 by Associate II
  • 1186 Views
  • 1 replies
  • 0 kudos

Resolved! How to generate header from .ucf file?

Hello,could you please clarify one topic for me. I am working with lsm6dsox sensor. How can I create a header (.h) file instead a .ucf to easily include in a project?I read that it is possible using Unico, but i didn't find this option in it. (Unico ...

YRakh.1 by Associate II
  • 1521 Views
  • 1 replies
  • 0 kudos

Resolved! Programming the sensor tile

Good day,I have purchased a sensor-tile and would like to code said tile. The board is receiving power and the SWD connections are correct and double checked. Then when the st link is plugged in and one wants to debug and program the micro an error s...

FBoth.1 by Associate III
  • 5199 Views
  • 8 replies
  • 0 kudos

lsm6ds3 Relative tilt function

the first interrupt is generated if the device is rotated by an angle greater than 35 degreesfrom the start position and remains in the blue zone for a period of time of at least 2 seconds1�?35 degrees. What is its principle calculation formula?At le...

ZhangTao by Associate II
  • 4923 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.