Resolved! Which SPI mode (CPOL, CPHA values) should one use with IIS3DWB and IIS2DH sensors?
SPI_MODE0 (0, 0)SPI_MODE1 (0, 1)SPI_MODE2 (1, 0)SPI_MODE3 (1, 1)
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
SPI_MODE0 (0, 0)SPI_MODE1 (0, 1)SPI_MODE2 (1, 0)SPI_MODE3 (1, 1)
In the datasheet, it says the gyroscope in the LSM6DSO is 1LSb = 70 mdps at +/-2000 dps full scale. I'm curious how this is obtained. For a signed 16-bit number I get 2000 / 32768 = 61mdps.For the accelerometer, 1LSb = 0.061 mg at +/- 2g full scale, ...
Hello everyone, i'm a beginner, I recently bought a STWINKT1. I'm trying to setup the HSDataLog, using the: '' quick start guide HS sensor dataLog application for STWINKT1. Running USB_DataLog_Run.bat the results is: no devices. I installed STM32Cub...
Connect STEVAL-STWINKT1 and PC. Execute USB_DataLog_Run.bat of 1.1 USB mode-command line example described in the user manual "UM2686". However, it says no device.
This module is advertised in manuals to several ST development boards, e.g. the 'F413 Disco.Why is there no product folder for this module?JW
The top line has the SR. Then there's a 3D barcode, then the number 010 or 919.
Hi, I recently acquired the STWIN board, working on predictive maintenance, High-speed data logging, Serial data logging applications.I need to interface an external temperature sensor DS18B20 using the one-wire protocol.I want to integrate my code i...
HiOut of the Box, there is a luxury firmware on board running, with many Sensors shown in the BLE App.But after flashing other example Projects, there is no code or binary file with the initial firmware.Where to get this?Greetings
Hey,we have a bunch of sensor tile.box boards, but they keep dying and needs to be refreshed with the OTA. - even with the newest FWis usually happens when we try to "play" a new app (made in expert view of the ST app)When is works, the data gets tru...
The chip is powered by an 3v3 LDO. I have measured the output, and there are no fall-outs. I suspect my I2C adapter to be doing it. On-board the I2C is pulled up to 3v3 by 2k2 resistors. But on the adapter the I2C gets pulled up to 5V also by 2k2 res...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.