MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DE substitute

Hi,We've got an old design with an LIS2DE sensor, but it is obsolete. Is there any part compatible pin-to-pin? Thanks in advanceBest regards,Manuel

ISM330DLC Bypass-to-Continuous mode problem

I am using ISM330DLC accelerometer, the FIFO mode is Bypass-to-Continuous and the trigger is WAKE_UP_SRC. When the bit OVER_RUN of FIFO_STATUS2 is set, I read x_data from FIFO, but all data is not correct. So I do a test, read x_data from FIFO when F...

Yzhen.1 by Associate
  • 1032 Views
  • 0 replies
  • 0 kudos

Resolved! iis3dwb data seems abnormal when in static

Below is the data for 3 axis data during static status. I feel it abnormal. It looks huge noise. is it normal? can you give some data if it is in static state.Acceleration [mg]:-161.28 -36.36 -923.78Acceleration [mg]:-126.88 -7.08 -941.84Acceleratio...

sming.1 by Associate II
  • 4913 Views
  • 6 replies
  • 0 kudos

Resolved! MEMS source for VS Code Cmake compilation on windows

Hi, I am using an STM32L4 Discovery kit and using VS Code on Windows 10 for development and using CMake to build the application. I have all the setup done using CMake. I now need to include the different mems middleware for calibration and need to k...

MRaj by Associate II
  • 2020 Views
  • 4 replies
  • 0 kudos

High current consumption on the LSM6DSM while checking for Activity

Hi,I'm using a LSM6DSM to detect periods of inactivity and put a MCU to sleep. Similarly, it uses the activity interrupt to wake the MCU. I observed an average current consumption of ~0.7 mA when configured to check for inactivity(Gyro enabled and OD...

GTS.1 by Associate III
  • 3858 Views
  • 9 replies
  • 0 kudos

About X-CUBE-MEMS

Hello,I have a few questions about X-CUBE-MEMS as following:Can we run multiple algorithms (MotionFX, MotionDI, MotionTilt etc) on the same platform simultaneously using the same input data? I would like to make performance comparision between algori...

JVinc.1 by Associate III
  • 2543 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.