2020-09-19 6:53 AM
Below is the data for 3 axis data during static status. I feel it abnormal. It looks huge noise.
is it normal? can you give some data if it is in static state.
Acceleration [mg]:-161.28 -36.36 -923.78
Acceleration [mg]:-126.88 -7.08 -941.84
Acceleration [mg]:-159.09 -25.86 -947.21
Acceleration [mg]:-147.13 -24.40 -943.79
Acceleration [mg]:-140.79 -15.62 -925.74
Acceleration [mg]:-157.87 -40.02 -936.23
Acceleration [mg]:-143.47 -20.50 -941.84
Acceleration [mg]:-142.01 -42.94 -940.62
Acceleration [mg]:-144.69 -28.30 -957.21
Acceleration [mg]:-154.21 -31.48 -916.46
Acceleration [mg]:-122.98 -25.38 -953.31
Acceleration [mg]:-150.55 -15.13 -949.40
Acceleration [mg]:-148.84 -16.84 -936.72
Acceleration [mg]:-160.55 -38.31 -917.93
Acceleration [mg]:-139.32 -23.42 -939.40
Acceleration [mg]:-150.06 -37.33 -921.83
Acceleration [mg]:-135.42 -13.42 -936.72
Acceleration [mg]:-162.75 -23.42 -940.13
Acceleration [mg]:-152.99 -1.46 -953.06
Acceleration [mg]:-169.82 -39.53 -931.35
Acceleration [mg]:-150.55 -8.78 -934.52
Acceleration [mg]:-161.77 -50.75 -918.66
Acceleration [mg]:-140.30 -9.76 -962.58
Acceleration [mg]:-165.92 -30.99 -942.82
Acceleration [mg]:-142.01 -7.08 -949.89
Acceleration [mg]:-176.17 -33.43 -946.72
Acceleration [mg]:-140.79 -16.10 -952.58
Below is the init sequence:
dev_ctx.write_reg = platform_write;
dev_ctx.read_reg = platform_read;
dev_ctx.handle = &SENSOR_BUS;
/* Check device ID */
iis3dwb_device_id_get(&dev_ctx, &whoamI);
printf("whoamI is %x\r\n",whoamI);
/* Restore default configuration */
iis3dwb_reset_set(&dev_ctx, PROPERTY_ENABLE);
do {
iis3dwb_reset_get(&dev_ctx, &rst);
} while (rst);
/* Enable Block Data Update */
iis3dwb_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/* Set Output Data Rate */
iis3dwb_xl_data_rate_set(&dev_ctx, IIS3DWB_XL_ODR_26k7Hz);
/* Set full scale */
iis3dwb_xl_full_scale_set(&dev_ctx, IIS3DWB_8g);
iis3dwb_pin_int1_route_t int1_route;
int1_route.drdy_xl = 1;
iis3dwb_pin_int1_route_set(&dev_ctx, &int1_route);
/* Configure filtering chain(No aux interface)
* Accelerometer - LPF1 + LPF2 path
*/
// iis3dwb_xl_hp_path_on_out_set(&dev_ctx, IIS3DWB_HP_ODR_DIV_800);
// iis3dwb_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);
iis3dwb_data_ready_mode_set(&dev_ctx,PROPERTY_ENABLE);
Solved! Go to Solution.
2020-09-28 12:51 AM
Thanks a lot, Eleon.
It is resolved by below changes
iis3dwb_xl_hp_path_on_out_set(&dev_ctx, IIS3DWB_HP_ODR_DIV_800);
iis3dwb_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);
-->
iis3dwb_xl_hp_path_on_out_set(&dev_ctx, IIS3DWB_XL_ODR_26k7Hz);
iis3dwb_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);
so I believe it is due to a wrong setting on filter related.
The data looks normal now with the interrupt enabled. There is some noise, but it is at least normal. The acc rms in static drops to 0.010 m/s2 now.
2020-09-22 8:17 AM
Hi @sming.1 ,
Are you facing the same issue also in the simple data read case, I mean without the INT1 pin configured? And on more than one device?
I cannot see something strange in the configuration, it is similar to the one available on Github, at this link: iis3dwb_read_data_polling.c.
-Eleon
2020-09-22 3:59 PM
Thanks, Eleon.
it looks much better when using polling in 10ms internal(see bottom log). so it looks like an interrupt related...
in interrupt handling, it is pretty straight forward as calling below function to read out the data.
iis3dwb_acceleration_raw_get(&dev_ctx, data_raw_acceleration);
i checked the odr with a gpio toggling in interrupt handler, it is 26.7 k about.
below is the spi init sequence.
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
Temperature [degC]: 25.05
Acceleration [mg]:45.99 75.58 -905.00
Temperature [degC]: 24.99
Acceleration [mg]:42.58 76.37 -904.87
Temperature [degC]: 24.98
Acceleration [mg]:43.07 75.40 -905.97
Temperature [degC]: 24.98
Acceleration [mg]:44.71 75.64 -910.36
Temperature [degC]: 25.01
Acceleration [mg]:43.80 74.30 -909.02
Temperature [degC]: 25.00
Acceleration [mg]:42.09 72.22 -899.38
Temperature [degC]: 25.04
Acceleration [mg]:42.94 75.88 -908.41
Temperature [degC]: 25.00
Acceleration [mg]:43.19 72.47 -913.17
Temperature [degC]: 25.00
Acceleration [mg]:45.51 74.48 -901.64
Temperature [degC]: 24.99
Acceleration [mg]:44.71 76.98 -915.85
Temperature [degC]: 25.02
Acceleration [mg]:44.53 75.27 -897.19
Temperature [degC]: 24.95
Acceleration [mg]:44.90 75.64 -908.17
Temperature [degC]: 25.00
Acceleration [mg]:44.29 75.76 -908.05
Temperature [degC]: 24.99
Acceleration [mg]:43.07 73.69 -900.91
Temperature [degC]: 24.94
Acceleration [mg]:44.04 74.97 -899.38
Temperature [degC]: 25.00
Acceleration [mg]:43.80 74.18 -905.00
Temperature [degC]: 24.98
Acceleration [mg]:46.42 76.74 -911.83
Temperature [degC]: 25.02
Acceleration [mg]:44.29 72.83 -908.78
Temperature [degC]: 25.02
Acceleration [mg]:45.99 72.77 -910.97
Temperature [degC]: 25.06
Acceleration [mg]:44.04 74.05 -908.17
Temperature [degC]: 25.02
Acceleration [mg]:45.87 72.71 -905.97
Temperature [degC]: 25.02
Acceleration [mg]:43.55 72.35 -901.82
Temperature [degC]: 24.98
Acceleration [mg]:39.28 74.66 -909.51
Temperature [degC]: 25.01
Acceleration [mg]:41.48 73.14 -904.87
Temperature [degC]: 25.02
Acceleration [mg]:42.70 78.45 -905.48
Temperature [degC]: 25.02
Acceleration [mg]:46.42 75.52 -901.70
Temperature [degC]: 25.01
Acceleration [mg]:44.29 75.03 -910.49
Temperature [degC]: 25.01
Acceleration [mg]:43.55 74.11 -909.27
Temperature [degC]: 24.98
Acceleration [mg]:42.70 73.81 -903.04
Temperature [degC]: 25.04
Acceleration [mg]:41.48 72.71 -902.56
Temperature [degC]: 25.01
Acceleration [mg]:43.68 71.98 -904.08
Temperature [degC]: 24.97
Acceleration [mg]:48.68 74.66 -906.28
Temperature [degC]: 25.02
Acceleration [mg]:43.68 77.84 -911.46
Temperature [degC]: 25.00
Acceleration [mg]:44.04 73.93 -907.92
Temperature [degC]: 24.98
Acceleration [mg]:43.62 74.54 -907.31
Temperature [degC]: 25.00
Acceleration [mg]:45.02 72.90 -908.17
Temperature [degC]: 25.02
Acceleration [mg]:43.92 77.90 -904.51
Temperature [degC]: 25.02
Acceleration [mg]:41.85 75.52 -906.09
Temperature [degC]: 25.01
Acceleration [mg]:42.70 75.76 -904.87
Temperature [degC]: 25.00
Acceleration [mg]:41.85 76.74 -906.70
Temperature [degC]: 25.02
Acceleration [mg]:42.15 76.01 -909.63
Temperature [degC]: 25.01
Acceleration [mg]:40.99 76.43 -908.05
2020-09-22 4:49 PM
when i just read whoami in interrupt handler, it always returns 0x7b, which is correct. so looks spi is no problem. seems the real data is not okay.
2020-09-24 9:08 AM
Hi @sming.1 ,
you may try to disable the BDU commenting the below line of your code, and see if something changes.
/* Enable Block Data Update */
iis3dwb_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
-Eleon
2020-09-28 12:36 AM
Hi @sming.1 ,
let me please add a couple of suggestions, in case they can be of some utility for you:
Btw, is the data polling reading procedure a possible workaround for you?
-Eleon
2020-09-28 12:51 AM
Thanks a lot, Eleon.
It is resolved by below changes
iis3dwb_xl_hp_path_on_out_set(&dev_ctx, IIS3DWB_HP_ODR_DIV_800);
iis3dwb_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);
-->
iis3dwb_xl_hp_path_on_out_set(&dev_ctx, IIS3DWB_XL_ODR_26k7Hz);
iis3dwb_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);
so I believe it is due to a wrong setting on filter related.
The data looks normal now with the interrupt enabled. There is some noise, but it is at least normal. The acc rms in static drops to 0.010 m/s2 now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.