MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have been using vl53l1x TOF sensor for finding distance. When I have tested in an open environment. I'm getting very unusual values, I'm not able to understand this values.

Could someone explain me what's going on when this sensor is placed in front of uneven surface such as stairs in open area. i'm attaching images of readings X-axis is sample number and y-axis is distance in mm. Samples are taken for every 100msec. Re...

0693W000004IF45QAG.png
Aperu.11 by Associate
  • 1778 Views
  • 2 replies
  • 1 kudos

VL6180x distance issue

Hi, We are using VL6180X to measure the cyclic movement of a part (a flat, white plastic sheet). The amplitude of this cyclic movement is about 20mm. The distance sensors work fine but we had two recent instances where the distance sensors returned a...

TBoul.1 by Associate
  • 1105 Views
  • 1 replies
  • 0 kudos

How do aI specify the .ioc file for X-CUBE-53L3A2?

I have added the X-CUBE-53L3A2 software package to STM32CubeIDE and successfully built and run the SimpleRanging sample application. I now want to make changes to the STM32F401 pin assignements (actually, add a second UART).When I click on the Nucle...

charles23 by Associate III
  • 1509 Views
  • 2 replies
  • 0 kudos

debug vl53l0x

someone knows ? when I start debug I've this error message ...

MSAMB.1 by Associate III
  • 1525 Views
  • 1 replies
  • 0 kudos

We're using the VL53L1X sensor and this will be sealed into our enclosure during the manufacturing process. Is there a humidity spec we need to be aware for the manufacturing process?

The enclosure this will be going into will be sealed and any humidity present during the manufacturing process will be trapped within the enclosure. Is there a humidity spec we should be aiming for?

DAmer.1 by Associate
  • 1186 Views
  • 1 replies
  • 0 kudos

Need help for the best ToF sensor selction for surrent device?

The built unit will need a sensor thats able to tell if either side of the gate is open, the unit will be mounted to one of the gate posts and will need to reach both gates during day and night. Prefered to be low power since it will be solar powered...

0693W000004I29lQAC.jpg
BHuiz.1 by Associate
  • 1016 Views
  • 1 replies
  • 0 kudos

Hi. I am trying to use the STEVAL-IDP003V1 module and have a compiler error for PROXIMITY SENSOR (the same for accelerometer and for inclinometer sensor). It seems that one struct definition is missing. Please, help me.

I have tried to compile the FW in the STSW-IDP003IOLDS library for temperature sensor without errors.Trying to compile, with IAR, for other sensors I always have an error about a missing struct definition.For example, the error is "Error[Pe020]: iden...

GRans.1 by Associate
  • 1124 Views
  • 1 replies
  • 0 kudos

Resolved! VL6180X 'New Sample Ready threshold' issue

Hi everyone,I have an VL6180X connected to a PIC18F46J50. VL6180X is powered to 3V3 and I have implemented I2C routines and application code as in https://cdn.sparkfun.com/datasheets/Sensors/Proximity/VL6180_ApplicationNote.pdf to work in single shot...

RCres.1 by Associate III
  • 1934 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.