MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to detect angular movement and wake up LIS2DW12

Hi, I have an LIS2DW12 fitted to a STEVAL-MKI179V1 board. I have it connected to a microcontroller programmed to set an interrupt pin on wake up as per DT0098. The interrupt pin goes high with a light tap in the xy or z axis. However I want it to det...

DSqui by Associate II
  • 2239 Views
  • 5 replies
  • 0 kudos

VL53L1X People Counting ROI center

I am implementing an “auto calibration�? of the ROI in my people counting algorithm based on the one provided by ST. The program defines the centers of the two zones used to detect entry/exit in an area. Currently I run a simple detection algorithm t...

HMull.1 by Associate II
  • 1402 Views
  • 3 replies
  • 0 kudos

X-NUCLEO-53L0A1 / VL53L0X Windows application not working

I am on my second X-NUCLEO-53L0A1 board, a replacement for the first board that suffered from the same problem. I have an STM32F401RE development board and I put the X-NUCLEO-53L0A1 board with its single detector only and I get as far as the Windows...

VL6180X wrap-around filtering: is this possible without the API?

Hello,I'm working on a project with a VL6180X ranging sensor, and I'm running into the problem that it responds to reflective surfaces far beyond the desired range (100 mm) - e.g. it picks up reflective stripes on the jackets of emergency personnel a...

RichardR by Associate II
  • 5175 Views
  • 12 replies
  • 0 kudos

Resolved! Can I connect multiple LIS2DS12TR to one SPI?

I need to know routin to use multiple LIS2DS12TR on one SPI if it's possible. If I undestood correctly nCS pin used to selecting between I2C and SPI mode. So if CS is high, SDO is open-drain. Is I need to simply connect SDO pins of LIS2DS12TR (may ...

Dfsd .1 by Associate
  • 1327 Views
  • 1 replies
  • 0 kudos

VL6180 register setup for use with cover filter

I am using the standard VL6180 Breakout Board from ST connected to a pyboard running micropython.For my application I need a range at least up to 200mm using multiple reflective surfaces from reflective to not so reflective. I have managed to get the...

GMcPh.1 by Associate II
  • 1106 Views
  • 2 replies
  • 0 kudos

Resolved! Merging of FP-IND-PREDMNT1 [WIFI] with AMicArray_UltrasoundFFT application. Has anyone tried it before?

Hi All, I am trying to merge FP-IND-PREDMNT1 [WIFI] with AMicArray_UltrasoundFFT application. Has anyone tried it before? Are there any suggestion or advice?More importantly I need to know if this is possible? are there any limitations?@Eleon BORLINI...

how to enable lsm6dsl i2c master,

When I enable lsm6dsl I2C as master , both lines are going to gnd. lsm6dsl_sh_master_set(&dev_ctx, PROPERTY_ENABLE);any tip on using lsm6dsl sensor hub, thanks

SRabi.1 by Associate II
  • 6433 Views
  • 10 replies
  • 0 kudos

Resolved! LIS3DH High Resolution Threshold

Hi Community,I am using Lis3dh sensor in 50HZ ODR, High Pass filter enabled with cut-off frequency 0.1 HZ with full scale range 8G and FIFO is enabled and set FIFO-to-Stream Mode.Case 1: I get interrupts for small events Normal Mode(HR bit is not set...

HPras by Associate II
  • 4442 Views
  • 15 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.