Resolved! LSM6DS3 PEDOMETER
Hi,I'm trying to read step counts. I'm executing all pedometer related functions, but I get no any output.Sincerely,TalhaAnd While Loop
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi,I'm trying to read step counts. I'm executing all pedometer related functions, but I get no any output.Sincerely,TalhaAnd While Loop
I understand the VL53L3 can detect multiple objects, and I think it puts ToF information into different buckets. Where can I find more information about this? app notes, register set, driver software, evaluation code? So far I can only see the data s...
We are running the sensor at 3V but the I2C is 1.8V. Does this mean the XSHUT is also 1.8V referenced. Does the XSHUT pull-up go to 3V or 1.8V?ThanksLeon
The random walk and bias stability of the LSM6DSM gyroscope could notbe found in the data sheet.Random walk , bias stability of gyroscope Please tell me the reference value.
Hello SThere am using STEVAL-MKI160V1 in which LSM6DS3 is placed and an trying communicate with it over SPI.Physical connections:CS- CSSCL- CLKSDA - SDO of mcSDO - SDI of mcVDD - 3.3VGND - GND SPI Configuration:SPI Freq- 1MHZSlave Select - Active low...
I would like to know what the accuracy of the embedded temperature sensor in LSM6DS3TR-C. However, I cannot find this information in the datasheet.
reference : https://www.st.com/resource/en/data_brief/vl53l1x-satel.pdfAs you can see, I have the names of the pins from the data sheet but I don't know which is pin 1 or pin 2 and so on
lis2mdl_reg.c has an error in the function int32_t lis2mdl_mag_user_offset_set(stmdev_ctx_t *ctx, int16_t *val).The function incorrectly calculates the OFFSET_X_REG_H, OFFSET_Y_REG_H, and the OFFSET_Z_REG_H registers because it converts val[0] to an ...
Hi, I want to use accelerometer using stm32f4 mcu with SPI protocol.The range is between 1 and 2 meters. Is this work good ?Thanks...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.