2021-05-26 9:50 AM
Hi!
I'm using lis2dw12 on a custom board and trying to acquire the acceleration based on the data ready signal that I routed to INT1.
The code was based on this repository but I think I'm doing something wrong because I can't get any signal from the pin while mesuring it with an oscilloscope.
Here's my configuration of the device.
lis2dw12_reg_t int_route;
/*
* Restore default configuration
*/
lis2dw12_reset_get(&dev_ctx, &rst);
lis2dw12_reset_set(&dev_ctx, PROPERTY_ENABLE);
do
{
} while (rst);
/*
* Enable Block Data Update
*/
lis2dw12_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/*
* Set full scale
*/
lis2dw12_full_scale_set(&dev_ctx, LIS2DW12_8g);
/*
* Configure filtering chain
* Accelerometer - filter path / bandwidth
*/
lis2dw12_filter_path_set(&dev_ctx, LIS2DW12_LPF_ON_OUT);
lis2dw12_filter_bandwidth_set(&dev_ctx, LIS2DW12_ODR_DIV_4);
/*
* Configure power mode
*/
lis2dw12_power_mode_set(&dev_ctx, LIS2DW12_CONT_LOW_PWR_LOW_NOISE_2);//LIS2DW12_CONT_LOW_PWR_12bit);
/*
* Set Output Data Rate
*/
lis2dw12_data_rate_set(&dev_ctx, LIS2DW12_XL_ODR_50Hz);//LIS2DW12_XL_ODR_100Hz);
nrf_gpio_pin_set (ACC_nSS);
// Enable data ready interrupt
int_route.ctrl4_int1_pad_ctrl.int1_drdy = PROPERTY_ENABLE;
lis2dw12_pin_int1_route_set(&dev_ctx, &int_route.ctrl4_int1_pad_ctrl);
nrf_delay_ms(10);I've checked CTRL7 register and the "INTERRUPTS_ENABLE" bit is set. Aside from that could there be any other way to check if the configuration is correct?
Thank you.
Solved! Go to Solution.
2021-05-27 8:01 AM
Hi @MRive.2 ,
first of all, I would disable the BDU bit in CTRL2(21h), so that you see continuous data incoming.
I think you can use lis2dw12_block_data_update_set(&dev_ctx, PROPERTY_ENABLE); with PROPERTY_DISABLE or something like that.
then, can you confirm you are able to read output data by accessing the output registers?
Niccolò
2021-05-27 8:01 AM
Hi @MRive.2 ,
first of all, I would disable the BDU bit in CTRL2(21h), so that you see continuous data incoming.
I think you can use lis2dw12_block_data_update_set(&dev_ctx, PROPERTY_ENABLE); with PROPERTY_DISABLE or something like that.
then, can you confirm you are able to read output data by accessing the output registers?
Niccolò
2021-05-28 5:36 AM
Hi @niccolo.ruffini ,
Thank you! It was precisely that! I checked CTRL2 register and BDU was indeed set, I just changed it with PROPERTY DISABLE and now I'm getting the interrupt signal.
Thanks!
2021-05-28 6:27 AM
Hi @MRive.2 ,
you are welcome =)
remember that you can "select a best answer" to help other user that may have similar issues.
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.