SensorTile.box upgrading firmware
Hi, I am getting errors for over the air upgrade. And want to do it manually but I can not locate the latest SensorTile.box SENSORTILE.BOX_v347.bin file, where is it on the website ? please help thank you
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi, I am getting errors for over the air upgrade. And want to do it manually but I can not locate the latest SensorTile.box SENSORTILE.BOX_v347.bin file, where is it on the website ? please help thank you
I am using NUCLEO-L476RG together with X-NUCLEO-CCA02M and following the quick start guide (slides 9-10)https://www.st.com/content/ccc/resource/sales_and_marketing/presentation/product_presentation/group0/77/e0/20/db/d4/65/42/cf/X-NUCLEO-CCA02M2_QUI...
Hi all,I am using LSM6DSL chip as a pedometer and sensing other stuff like tap detection, tilt detection etc on a wearable device. The pedometer counts are pretty close to accurate when I compare it with other standard devices like the apple watch/ f...
My Senosr board is on the table with no vibration event applied to it. Instead of seeing a value of zero or something close to zero, I am reading the X, Y, Z values as ( X=476, Y=52676, Z=10472).What is the issue here and how to fix it?My Setting is ...
Hi, Does Edge Impulse supports Steval-MKSBOX1V1 Sensor Tile Box? regards,Shankari
Hello there, I am currently using LIS2DTW12. In the datasheet, it states the accuracy of temperature sensor is 0.8 degree C(typ.), I notice the temperature reading has +/- 3 degree C among 10 LIS2DTW12 units. Is it normal? I also wonder if the LIS2DT...
Hi, regarding the STEVAL-MKI208V1K, what is the purpose of the pins CSX, SDX, OSDO and OCS?In the diagrams of the Data brief available from the web page, it can be seen that those pins actually are not coming from the IIS3DWB pins.I want to connect t...
Hello,I'm using a IIS3DWB in my design.As indicated in datasheet, RES pins (10 and 11) should be connected to VDD_IO or leave unconnected (Table 1: Pin Description).However, the STEVAL-MKI208V1 have RES pins tied to GND (Figure 1 STEVAL-MKI208V1 boa...
Hello,My company is using since more than one year a combination from HTS221 and stm32f407 uController , I2C is used.The problem is that on some devices i have from the sensor different results.also some sensors give correct output where the others g...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.