MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! On the STWIN SensorTile Wireless Industrial Node, the standard en.fp-sns-datalog1_v1.2.0 firmware behaves differently if using the binary, rather than compiling the code in the STM32Cube IDE.

When I compile the code in the IDE and run it (with the acquisition json file set to activate for 5s, then idle for 10s, and repeat) It activates correctly the first time. However, when coming out of idle the second time, it produces an SD card erro...

0693W00000DmSBZQA3.png
LWeir.775 by Associate II
  • 1694 Views
  • 2 replies
  • 0 kudos

LSM6DSM factory reset

I have been working with this sensor for a while. It started to give weird errors such as reading all zeros on all axis. Then sometimes it would initialize but read values like 4, 0, 4 and such. Which is impossible in a static position. I have tried ...

FBoth.1 by Associate III
  • 3365 Views
  • 5 replies
  • 0 kudos

VL53L3CX detects no targets

Dear STM-Team,our first custom boards with VL53L3CX just arrived and I’ve ported the API to Zephyr (already did that for VL51).I can see that the comms work, because I can read the chip id and start the mandatory calibrations as well as the measureme...

CSchr.14 by Associate II
  • 4172 Views
  • 8 replies
  • 0 kudos

Resolved! LSM6DSO32X driver

Hello,I'm looking for the drivers for the LSM6DSO32X. In the example code I found the drivers for LSM6DSO32 and for LSM6DSOX which are similar but not identical. Are them available somewhere?Davide

DGiov.1 by Associate III
  • 3509 Views
  • 5 replies
  • 0 kudos

FIFO Corruption on LSM6DSM

There appears to be a hardware bug on the LSM6DSM where if a sample is acquired while reading from the FIFO, then the pattern # becomes incorrect. I can consistently replicate this issue by reading at random intervals. Additionally, data on the FIFO ...

JBarr.12 by Associate II
  • 7179 Views
  • 7 replies
  • 1 kudos

LIS2DW12 temperature reading fluctuates

Hi,I have created a small function that reads out the 8-bit temperature register in the lis2dw12 sensor. The code is shown belowstatus lis2dw12::temperature(int8_t *temp) { *temp = static_cast<int8_t>(read_reg(REG_OUT_T)) + 25; printf("%d\r...

0693W00000DmdcgQAB.png
CThue.1 by Associate II
  • 1788 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.