MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! X-NUCLEO-CCA02M2 interface with nucleo-f401RE

Hi, I am using X-NUCLEO-CCA02M2 microphone board with nucleo-f401RE for USB audio streaming. Can anyone share the details about interfacing pin connection(which I2S pin is used)?. My understanding is like timer is used to connect pdm clock with I2S...

KK Y.1 by Associate II
  • 1893 Views
  • 1 replies
  • 0 kudos

Resolved! Allowed values for interrupt threshold of LIS2DH12

Hi, I am using a LIS2DH12 chip to detect the orientation(in 3D space) of a device.For this purpose I'm using the INT pins in 6D position mode to generate interrupt signal/s, that will alert me if the device has exited/entered a known positional area....

ilg by Associate
  • 1970 Views
  • 2 replies
  • 0 kudos

Resolved! High-pass path: BW_FILT setting

When BW_FILT[1:0] = 00, it's different between AN5201 AND DATASHEET. Which one is real?​in AN5201:In Datasheet(DocID031788):​​

0693W00000FBx7wQAD.png 0693W00000FBx8BQAT.png
user1 by Associate
  • 1122 Views
  • 1 replies
  • 0 kudos

Resolved! Unable to initialize X-CUBE-MEMS1 libraries

I'm using a NUCLEO-L476RG with a STEVAL-MKI197V1, connected in SPI mode without any expansion board. My setup works: I successfully used the LSM6DSOX low-level driver to read sensor data. But my attempts to use the high level libraries, such as Motio...

paul19 by Associate III
  • 3559 Views
  • 6 replies
  • 0 kudos

Resolved! IIS3DWB static and dynamic noise question

Hello ST team, I’m using the IIS3DWB (STEVAL-MKI208V1K) together with an Arduino Portenta H7. No filter added through the composite group of digital filters, only the default LPF1. Also, 2g scale resolution.When placing the sensor on a surface isolat...

FCook.1 by Associate III
  • 3213 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.