MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Questions about filtering & thresholds in the LIS2DH

I have a question about the high-pass filter mode configuration. With the configuration at 0x00, it states in the data sheet that the high-pass filter mode will be in normal mode in which it will be reset by reading the REFERENCE register. Assuming t...

IC.1 by Associate II
  • 2102 Views
  • 2 replies
  • 0 kudos

Resolved! How to distinguish LSM6DSO32X from LSM6DSOX by software?

Hi,how to differentiate both chips, if they have the same value for WHO_AM_I register?I know that I could read couple times the accelerometer values, calculate magnitude over all axis and check if the value is near 1g or 0.5g (assuming no movement du...

MMade.1 by Associate II
  • 1336 Views
  • 1 replies
  • 0 kudos

Burning up of STEVAL-STLCS01V1.

Hello Folks,Greetings. I have been using STEVAL-STLCS01V1 on one of my IoT project and for some reason have burnt a few of them. I am pretty sure there is no short between the pins as well as no design issue. Has some one faced something similar? It ...

SJosh.8 by Associate
  • 1592 Views
  • 3 replies
  • 0 kudos

Why current of LIS2DTW12TR is too high?

Hi,We are trying to measure total current of LIS2DTW12TR. We have circuit board which according to schematic in details. We have 60uA when we measure the current flowing on CN34.  But in the application notes of LIS2DW12 ( i know it is a different mo...

0693W00000FCHaeQAH.png

AN5201: ODR

Output Data Rate(ODR) It can be considered as the frequency of data update, and the data will not be updated between update intervals.

user1 by Associate
  • 1175 Views
  • 1 replies
  • 0 kudos

Resolved! problem with lsm6dsl free fall detection

Hi sir , I working with( LSM6DSL)STEVAL-MKI178V1 Dk board communicating with nrf52840 controller board.i am able work pedometer and significant motion and tilt detection these modes are working but i am trying to generate free fall detection but i am...

MRedd.3 by Associate II
  • 2312 Views
  • 3 replies
  • 0 kudos

I want to use two wake up inrterrupts at the same time. Thresholds and duration will be different. I cannot use it at the same time because I changed the register value while doing the settings.

I want to use wake up interrupt for two different thresholds at the same time,for example I want to give wake up threshold 1g for interrupt 1, I want to give 500 mg for interrupt 2. And duration will be different.I change the value of WAKE_UP_THS, W...

Iakgu.1 by Associate III
  • 1072 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.