Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
May I know differences between sensors above? Looking from parametric table, seems the same...Thanks.
I'm using a Jetson Nano, and am trying to get it running though python. Extreme lack of documentation and references for the board has left be confused.Making the generic connections and running i2cdetect in the terminal, I detect the device at addre...
I am using Keil for firmware developmentCurrently I don't have a Nucleo board with me
Hello ST,I am using the Unico 9.11.0.0 version software (STEVAL-MKI109V3 board) with STEVAL-MKI178V2 ( LSM6DSL ) Sensor board.from this link- https://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/configuration_examples/exampl...
The description of the threshold registers says: "The value is expressed in 15-bit unsigned. Even if the threshold is expressed in absolute value, the device detects both positive and negative thresholds.".There is only one threshold to be set, desp...
Hello.I am trying to perform temperature calibration on ISM330DHCX (bought from adafruit) for both gyro and accel.IMU is sampled at 104Hz via SPI bus.The IMU sits inside a glass container, and is placed in a freezer. When the IMU temperature reaches ...
Hi, I am looking into using the LIS3MDL 3-Axis Magnetometer in an application with high frequency oscillating magnetic fields. I have looked through the datasheet of the LIS3MDL and it seems to meet most requirements that I've checked. My application...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.