MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

4-20ma or 0-10v dc to 0-3.3 analogue ip of STM32 circuit?

I want to interfacing industrial analogue sensors with STM32F030C8T6TR so I need to convert signal in to 0-3.3v signal.4-20ma to 0-3.3v0-10v to 0-3.3v​1) For converting signal which is good way using opamp or voltage divider?​​2) It is possible using...

Resolved! I am using the STEVAL-STWINKT 1B having downloaded the latest STM32CubeFunctionPack_DATALOG1_V1.3.0 as verified by the Device List of the ST BLE Sensor v 4.14.4(76) The app shows an error of "Board scanning timed out" in playing the Example Apps.

The device is recognized by the smartphone, but is unable to pair with it even though the ST BLE Sensor recognizes and does connect and download its configuration and provide battery level. It indicates that it is logging DAT files to the SD card and...

DDown.1 by Associate II
  • 1914 Views
  • 2 replies
  • 0 kudos

STM32F4 Discovery kit I2C communication with LSM303DLHC.

Hi Team, I want to learn the i2c features and functions while using STM32F4 Discovery kit based on STM32F411VE and communication with LSM303DLHC.I want to know if there is any deault register selected in LSM303DLHC when no register value is mentioned...

IJose.1 by Associate II
  • 986 Views
  • 0 replies
  • 0 kudos

Linux Driver for MP23DB01HP PDM Digital Microphone

I'm looking for instructions on interfacing MP23DB01HP Microphone to Cortex-A7 on STM32MP157 through I2S bus.The application note AN5027 is a good starting point but does not mention how to integrate with Linux on Cortex-A7.I've modified the devcie t...

farid by Associate II
  • 3617 Views
  • 2 replies
  • 0 kudos

H3LIS331: SPI read response is always 0x00

Hello, I am attempting to communicate using SPI with an H3LIS331 accelerometer. The H3LIS331 is on a custom board that originally had a LIS3DSH on it. The LIS3DSH had been working without a problem, but we were looking to expand the acceleration scal...

MRigg.1 by Associate
  • 4684 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.