MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IIS3DWB in fifo mode does not work

HelloI am using an IIS3DWB mems for continuous acquisition.So I configured it to use fifo and interrupt.But, during transfert, I see INT1 going high, and transfert aborts.See Capture.png.Please find IIS3DWB configuration in Config.c, is it good?Thank...

DLafo.1 by Associate II
  • 3199 Views
  • 2 replies
  • 0 kudos

Resolved! Can LIS2DW12 be configured to present TAP interrupt and to give XYZ acceleration values on demand at same time?

Please,give me your opinion.I have to develop an anti-tamper board.By now I was asked to select one of 2 working modes:1)Interrupt on TAP2)XYZ values on demand ,microcontroller periodically checks variations in XYZ values.Is it possible to have both ...

LIS3DML Interrupt setup. Latch/No Latch not working as expected

I have a project using the LIS3DML Magnetometer. I am looking for a behaviors where the Interrupt lines only stays high or low ( depending on settings) as long as the configured thresholds are true. From what Iv tested. Looking at Z only when interr...

JVan .6 by Associate
  • 1586 Views
  • 2 replies
  • 0 kudos

Resolved! How can i get Euler Angle's

Hi i am using STEVAL-MKI182V2 evaluation board and i am having a doubt that in this PDF dt0060-exploiting-the-gyroscope-to-update-tilt-measurement-and-ecompass-stmicroelectronics.pdf at purpose and benefits para, it is mentioned that This design tip ...

Anil3 by Associate III
  • 2141 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DTW12 Aliasing cut off

Hello,I'm using an LIS2DTW12 and I don't understand very well which is the cut off frequency.I'm quite confused because from this picture seems that the anti aliasing filter has cut off frequency fixed to 400 Hz : Then in this table the cut off frequ...

0693W00000NrRQ4QAN.png 0693W00000NrRQ9QAN.png
RStra by Associate III
  • 2573 Views
  • 3 replies
  • 0 kudos

Resolved! can't able to understand the raw_data ISM330DLC

Hi Everyone,I am new to this field and working on ISM330DLC i am using the below program (link) to read the data and getting the raw_data of gyroscope values aways 0 when i kept on table it is getting values only if i made any movement. but i read t...

Nani by Associate II
  • 2393 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.