2022-06-02 4:53 AM
Hi Everyone,
I am new to this field and working on ISM330DLC i am using the below program (link) to read the data and getting the raw_data of gyroscope values aways 0 when i kept on table it is getting values only if i made any movement. but i read that gyroscope will return some offset value when there is no movement in that case the program which i am using is it wrong?? but it is given the ST only in github what might be wrong can't ale to get.
Solved! Go to Solution.
2022-06-03 2:31 AM
Hi @Akuma.6 Nallala ,
I believe this is correct, you are reading almost 0 LSB (equals to 0 dps) on all the 3 axis when the device, and in particular the gyroscope, is in rest condition. It is different for the accelerometer, since typically the Z axis shows 1g offset when the device is pointing towards the ceiling. For the gyro, if you oscillate your hands, you should see something similar to a sine waveform plotting the dataout.
The drivers you are linking are the correct one: in particular, here below I reported the formulas for LSB to physical unit conversions, for both axl and gyro.
/*accelerometer LSB-to-physical units conversion*/
float_t ism330dlc_from_fs2g_to_mg(int16_t lsb)
{
return ((float_t)lsb * 0.061f);
}
/*gyroscope LSB-to-physical units conversion*/
float_t ism330dlc_from_fs125dps_to_mdps(int16_t lsb)
{
return ((float_t)lsb * 4.375f);
}If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2022-06-03 2:31 AM
Hi @Akuma.6 Nallala ,
I believe this is correct, you are reading almost 0 LSB (equals to 0 dps) on all the 3 axis when the device, and in particular the gyroscope, is in rest condition. It is different for the accelerometer, since typically the Z axis shows 1g offset when the device is pointing towards the ceiling. For the gyro, if you oscillate your hands, you should see something similar to a sine waveform plotting the dataout.
The drivers you are linking are the correct one: in particular, here below I reported the formulas for LSB to physical unit conversions, for both axl and gyro.
/*accelerometer LSB-to-physical units conversion*/
float_t ism330dlc_from_fs2g_to_mg(int16_t lsb)
{
return ((float_t)lsb * 0.061f);
}
/*gyroscope LSB-to-physical units conversion*/
float_t ism330dlc_from_fs125dps_to_mdps(int16_t lsb)
{
return ((float_t)lsb * 4.375f);
}If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2022-06-03 5:31 AM
Hi @Eleon BORLINI
Now i can able to get data from library motionGC_update function data.out is coming but the bias is not updating it is showing zero always even thought it is placed in steady position what might be the reason?
2022-06-09 11:18 PM
Hi @Eleon BORLINI
In my application i am using the Motion_DI library and getting values of rotation, quaternions, gravity and liner acceleration. How can i validate that data
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.