2022-12-23 10:25 AM
I would like to use the MotionFX Library from the X-CUBE-MEMS1 package in a project on a STM32WL55JC.
The datasheet of the library states the following:
I have already written a library for another application that converts my data for the MotionFX library and returns me the filtered values (Similar to User Manual UM2220, page 14). Before I include this, I have 8.66 KB of free RAM and 38.91 KB of free Flash. When I add the functions with the MotionFX Lib, I get the following errors:
Now my questions:
Best regards.
2023-01-13 8:03 AM
Hello,
The code size (in FLASH memory) cannot be decreased anymore because the library has been already compiled with highest optimization for size. I've analyzed the size for the most memory consuming Cortex-M4 library which is MotionFX_CM4F_wc32_ot_hard.a and it occupies 41.5 kB of FLASH and 2.2 kB of RAM. If you have 39 kB of FLASH free then it cannot fit. In case of RAM it's a bit tricky. The library itself really consumes 2.2 kB of RAM (sorry for obsolete value of 1.1 kB in UM), but all the variables needed for the library usage are now due to support of multiple instances of library moved outside the library so once you use the library you create all these variables in your application which consumes more RAM than you have.
Best regards,
Petr
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.