MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-l475E-IOT01A connection for unico GUI with LSM6DSOX

Hello,I am trying to develop an audio classification through a decision tree in unico GUI platform using the mlc for lsm6dsox. I have the B-l475E-IOT01A motherboard and I want to know if it is possible to use the sensor LSM6DSOX with this motherboard...

SRodr4_0-1690999603521.png
SRodr.4 by Associate II
  • 997 Views
  • 0 replies
  • 0 kudos

Reading bad data from LIS2MDL using 3-wire SPI

Sensor: LI2MDLMCU: STML072I am trying to read the who_am_I register (register 0xAF) with the 3-wire SPI setup, but it is returning the wrong data.Below is a screenshot of the transmission and the return from the LIS2MDL. The transmission's first bit ...

Cfaya1_1-1690604682247.png
Cfaya.1 by Associate II
  • 2536 Views
  • 2 replies
  • 0 kudos

Resolved! DRDY not returning low on AIS2IH

I am using the AIS2IH and polling the DRDY bit of STATUS to see when a new sample is available .  I am using single data (on demand) mode and ODR bit is set.  The spec sheet says that DRDY returns low after the high part of X,Y or Z has been read, bu...

Resolved! Multiple STHS34PF80 on I2C bus

I have an application that requires two STHS34PF80 sensors on the same I2C bus. I tried using N-FETs on the SDA lines to select between them but this doesn't work, not sure why. I will try the 3-wire SPI bus but I am not sure my current MCU API supor...

KWine by Senior
  • 2542 Views
  • 3 replies
  • 0 kudos

Resolved! IMU LSM6DSO FSM Settings

Hello Team ST,I would like to have your guidance on setting a FSM for wrist tilt application. At the moment, we use following FSM settings as per the code here.Link: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/v2.00/lsm6dso_S...

ASoni2_0-1690543414543.png ASoni2_1-1690543657397.png
ASoni.2 by Associate III
  • 1683 Views
  • 1 replies
  • 0 kudos

LSM6DS3TR-C Reading more than one pattern from FIFO

Hi,I'm working with a LSM6DS3TR-C.Currently I've a working app where I configure a FIFO threshold for accel, gyro and timestamp data, and a THS interrupt in INT1.Once the interrupt occurs, I can read all the patterns, one at a time like this:  #de...

Martxel by Associate
  • 1751 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.