MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! AIS2DW12 Zero-g level offset accuracy, long term

Can anyone tell me how to understand the following parameter out of the AIS2DW12 datasheet.Zero-g level offset accuracy, long term: ± 700mgWhen i use the sensor with a resolution of ± 2g, then I hope there ist not the possibility that the offset will...

dmeise by Associate II
  • 2023 Views
  • 2 replies
  • 0 kudos

LIS2DW12 slow activity detection

Hello everybody,In the AN5038 it is well described how to setup the internal state machine to detect activity, but it has does not fit my need:If I have my  product in my hand, I want detect slow motion in 3 XYZ axes, but if my product is on my desk ...

LSM6DSO - Sensitivity to vibration.

Hi, I am trying to integrate LSM6DSO in an iOT and would like the LSM6DSO raise wake up interruption when iOT is moved (with a normal movement). Now my problem is the following :I programed my interruption and it's run. I can detect the motion on my ...

egeo by Associate
  • 1414 Views
  • 1 replies
  • 0 kudos

IIS3DWBTR power down to wake up process

Hi,We have achieved lowest current consumption(5.5uA) in power down mode as per datasheet with the pin configuration.Now we are trying to wake up from power down mode,By enabling the accelerometer CTRL1_XL register-101_Value ,but still module is in p...

nandhinis by Associate II
  • 1878 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSOX SPI read and write protocol in mode 1

Hello! I would like to check if the SPI read and write protocols in mode 1 are the same as those in mode 3 (as suggested on the datasheet). If they're different, may I know what the differences are?Thank you!

Resolved! LIS2DW12 Output Values

Hi experts,I am working with the LIS2DW12 accelerometer and the AN5038 document mentions the function to calculate the output values of the axis. 2g is mentioned, but what about 4g, 8g and 16g? Is the factor "4" the same for all scales?Thank you in a...

TVela1_0-1690469523903.png
TVela.1 by Associate III
  • 1695 Views
  • 2 replies
  • 1 kudos

How to evaluate IIS2ICLX?

I Am building an Inclinometer for tilt sensing with IIS2ICLX and want to evaluate this sensor, so can you Please suggest the Required Material for the same, Like Evaluation board, Mother board required, Software required.*Edited by moderation, please...

DChou.2 by Associate
  • 1798 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.