MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Shock Survivability

What does "shock survivability" of a module mean ? Does it imply that the module reading with not change when the module exceeds the threshold value or will exceeding the limit kill the module ? For an application of +-25g , which IMU and pressure se...

H3LIS331DL

Hi,I readed the default value of the identification register in H3LIS331DL by SPI mode and it responded with 0x32h as per the data sheet,but while reading the STATUS REG default value it responded with 0xFFh instead of 0x00h. How it's possible one re...

Gokulraj by Associate II
  • 2193 Views
  • 2 replies
  • 0 kudos

Cannot open UNICO-GUI pkg on MacOS Ventura

When trying to download either Unico-GUI 9.14.6 or 9.13.0 I keep getting the error below. Any idea how to solve that on MacOS Ventura? I have already tried opening the pkg with control+right click, etc. with no success.  

andfer by Associate
  • 3980 Views
  • 2 replies
  • 3 kudos

LSM6DSM- Incorrect Accel Data on high ODR using FIFO

Good day, I'm currently reading data on the FIFO using Continuous-to-FIFO mode. I'm also using the lsm6dsm_STdC provided on Github. I'm doing the tests using the STEVAL-MKI189V1I've set up the FIFO to only read Accelerometer data for now. While testi...

x-down.png y-down.png z-down.png

Is there a reference platform available for ScanAR

Is there a reference platform available for ScanAR as mentioned here?https://www.st.com/content/st_com/en/about/innovation---technology/mems-scanar.htmlOur reference designAdditionally, to ensure a faster and a swifter integration cycle, ST develo"

NPete.3 by Associate
  • 1828 Views
  • 2 replies
  • 2 kudos

Couldn't initialize MotionCP library

I have connected X-Nucleo-IKS02A1 to Nucleo H563Zi.When I am trying to initialize the MotionCP library using MotionCP_Initialize() function, it is not getting initialized and I couldn't step into it.But when I initialize IKS02A1_MOTION_SENSOR_Init(IK...

Priyaa by Associate II
  • 1098 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.