MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Indoor location GPS tracking using LSM6DSR sensor

Greetings to everyone, I would like to ask you for help. I want to track GPS in a closed position. I get latitude and longitude information from GPS in an open area. In a closed position, I want to get location information with the accelerometer and ...

ST tile box pro sampling time issue

Hi all ,                I have stored IMU quaternion data into the SD card. I did use the Algo builder tool for that. I couldn't get the samples in configured 100Hz. Kindly help to store all samples in 100hz rate. 

sampling time issue.png

Resolved! LSM6DSO VDD and VDDIO sequencing and dependancy

Good dayI am using LSM6DSO with 3V3 VDD and 1V8 VDDIO.Can the supplies(VDD and VDDIO) be ON/OFF independently or is there a requirement for one of the two to be ON before the other?In my instance the VDD might come on before the VDDIO and in other ci...

AWolf.3 by Associate
  • 1618 Views
  • 1 replies
  • 1 kudos

Resolved! ILPS22QS data ready interrupt

Hi, I need clarification about interrupt on ILPS22QS barometric pressure sensor.My test project involves LIS3MDL and ILPS22QS connected to MSDA and MSCL on LSM6SDO, which is connected to an mcu in 4-wire SPI interface, to use sensor hub on LSM6DSO (I...

el659 by Associate III
  • 2491 Views
  • 3 replies
  • 1 kudos

Using STEVAL-MKI236A with UNICO GUI

Hello,I have STEVAL-MKI236A (ASM330LHB - IMU) evaluation board, How can I make use of the UNICO-GUI to interface with the board. I do see the board listed on the GUI but how will I be able to interface with gui with just I2C without using the MOTHERB...

LIS2DU12TR accelerometer

Hi.  I used LIS2DU12TR accelerometer IC on the PCB.  It's angle value  was changing every sec. but my smart phone app indicated current angle is 0.0 degree.    current angle is -0.515648[proc_bt_read_all] TX data (len=15)00 00 02 00 00 00 00 00 00 7F...

LogosLEE by Associate
  • 3420 Views
  • 4 replies
  • 0 kudos

About MotionFx library

I want to calculate the displacement using the MotionX library with the LSM6DSR sensor on the stm32. For example, I want to write a code that calculates the displacement when the sensor moves 20 cm to the right on the table or calculates the displace...

h3lis200dl consumes too much power.

When I used the IIC communication mode of h3lis200dl, I connected the 7th pin SDO directly to the ground. Since the SDO pin has a pull-up resistor inside, the current is too large (about 60uA). I would like to ask if there is an unopened register to ...

132.png
Phoenix1 by Associate
  • 1860 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.