MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Microphone self noise IMP34DT05

Hello,I'm using the IMP34DT05 microphone and it records fine but there is always a noise overlapped and it is very annoying.I have tried recording the background noise in anechoic chamber (see attached audio, high-pass filter alpha is 0.98). Do you k...

frnt by Senior
  • 2496 Views
  • 3 replies
  • 0 kudos

Resolved! I2C with IMS330dlc

Hi I am new to the I2C communications. I am trying to communicate to the IMS330dlc chip. I am using a lab jack U3-HV.. I am programming this via Visual Studio 2022 using c# code. I cant get back the 106 for Who am I. below is the code that I setup on...

Resolved! Clarification Request: LSM9DS1 On-Board Sensor Fusion

Hi all, I’m confirming whether the ST LSM9DS1 provides any on-board sensor fusion output (for example quaternion/Euler), or if fusion must be done on the host MCU. If anyone has definitive guidance from ST docs/support, please share. Thanks.

Resolved! Help with top marking code for LSM6DSOXTR

Hello, I work on quality control for a company and I need to create an instruction of incoming for the item PN  LSM6DSOXTR, but I can't find any documentation about the topmarking of this item.It is mark on the item S4QR CODE504Is the "S4" the markin...

Resolved! A3G4250D Junction Temperature and Thermal Resistance Data

Dear STMicroelectronics Technical Support Team,I am currently working on reliability calculations for a design that incorporates the A3G4250D gyroscope. For accurate thermal and lifetime analysis, we require the following parameters:Maximum junction ...

Resolved! LSM6DSO FIFO read optimization

Hello.I'm working on product with LSM6DSO IMU.I have the communication working, but I'm trying to optimize a reading of the FIFO buffer.In the AN5192 document there is sentence: "The wraparound function from address FIFO_DATA_OUT_Z_H to FIFO_DATA_OUT...

Bennny by Associate III
  • 380 Views
  • 1 replies
  • 0 kudos

LSM6DSV320X LPF2 not working

Hi Because our recorded LG acceleration data shows strong aliasing artifacts we tried differten sensor configurations but nothing realy helped. Even worse we coud not see any effect of the LPF2 filter despide ODR and filter frequency settings. So we ...

LSM6DSO analog anti aliasing

Hi,I would like to confirm if setting LSM6DSO ODR to 6.66KHz and LPF2 to ODR/10 (resulting to 666Hz bandwidth), then setting a FIFO decimation factor of 8 (resulting to 833hz FIFO ODR) will work in preventing aliasing for signals above 417Hz? We have...

adrianT by Associate II
  • 1397 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.