MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RoHS of STEVAL-MKI208V1K

Dear Sir or Madam,I require a RoHS declaration of conformity for the following component:STEVAL-MKI208V1KCould you please share it?Thank you very much and kind regards,Thomas

Cem187 by Associate
  • 337 Views
  • 3 replies
  • 0 kudos

LSM6 Wakeup on Gyro-Z Threshold

In the past, I have used an LSM330 to wakeup on a gyro z-axis threshold and activate the INT1 pin as shown below:Gyro_WrByte(GYRO_CTRL_REG1, 0x3f); // 95Hz DataRate : 25Hz Cutoff : Normal Mode : Enable All AxesGyro_WrByte(GYRO_CTRL_REG2, 0x07); // HP...

Yashu by Associate
  • 365 Views
  • 3 replies
  • 0 kudos

Resolved! LSM9DS1 EOL Guidance & 9-Axis IMU Fusion Recommendations

After reviewing the website, we noticed that the LSM9DS1 is currently listed as obsolete. We would therefore appreciate your guidance on the following points:Is the LSM9DS1 still recommended for new designs, or should it be avoided given its obsolesc...

Asm330Lhh DEVICE_CONF

Hello, I have encountered some issues while developing with the  ASM330LHH. During the initialization sequence of the ASM330LHH interface, I first read the WHO_AM_I  register. After confirming that the value is correct, I proceed to access other regi...

wz2 by Associate
  • 296 Views
  • 2 replies
  • 0 kudos

Resolved! LIS3MDL calibration issues

I'm using a LIS3MDL magnetometer on my board, and I figured out how to calibrate it to account for distortions  caused by the board, and the procedure works. However, it seems that every time the same magnetometer is turned off and re-powered, the me...

bu by Associate
  • 251 Views
  • 1 replies
  • 0 kudos

Resolved! ST1VAFE3BX vAFE validation against reference signals

I'd like to validate ST1VAFE3BX vAFE measurement data against test signals as part of hardware design validation of a custom ECG sensor design based on ST1VAFE3BX. I intend to input reference signals (differential or single ended) into the two bio ch...

bwilkins by Associate II
  • 966 Views
  • 6 replies
  • 0 kudos

LIS2MDL (LGA-12L) Leakage current

Hi Team,We have designed and manufactured several thousand PCBs that include the LIS2MDL (LGA‑12L) sensor. All boards are functioning correctly from an operational standpoint. However, because our devices run on battery power, load current is critica...

Mallik18 by Associate II
  • 775 Views
  • 8 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.