MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12 - Changing FIFO mode from bypass to cont-to-fifo

GreetingsI am running an application where I am using the LIS2DW12 accelerometer. I am using it for classical sampling of acceleration values in cont-to-fifo mode, which works fine. The FIFO is configured with the High pass filter enabled. I now want...

ZAIDS-S23 by Associate III
  • 2360 Views
  • 2 replies
  • 0 kudos

LIS3DH sensor data offset/value problems

We have designed the LIS3DH onto a custom PCBA, and we are seeing some oddities with the sensor readings post manufacturing. The PCBA goes into a two part injection molded enclosure made of ABS, and the two halves are ultrasonically welded together. ...

LSM6DSR use FIFO mode read data failed

I use LSM6DSR,  I set Accelerometer ODR selection can read data, but i choose fifo mode to read data, i don't read data, i set CTRL3_C is 0x01, CTRL1_XL is 0x50,  CTRL3_C is 0x40, CTRL5_C is 0x20, CTRL9_XL is 0xf8, INT1_CTRL is 0x01, INT2_CTRL is 0x0...

sunyu by Associate
  • 1394 Views
  • 1 replies
  • 0 kudos

ISM330DLC Lifecycle

Hi all,I wanted to get information on the lifecycle of the ISM330DLC device? Is there a certain date when the sensor values will drift outside of the allowable tolerances? Thank you,Imran

IKalh.1 by Associate II
  • 2967 Views
  • 4 replies
  • 0 kudos

BLE connection allmems 1 v4.2.0 - Sensortile

Hello, I'm using a STEVAL-STLKT01V1 demo board to perform voice streaming over BLE using allmems 1 v4.2.0 (since versione 4.3.0 dropped support for my demo board). My setup is:Steval demo board with allmems v4.2.0Python script using Bleak library to ...

Resolved! LSM6DSL + LIS2MDL noise in one acceleration axis

Hi,I am using the setup with LSM6DSL + LIS2MDL. All works fine, with the exception that once started the conversion to FIFO with sensor fusion, at 104 sps, I observe significant periodical (around 22 samples cycles) noise on the last acceleration axi...

ism330dhcx - 6dof position + orientation estimation algorithm

im using the ism330dhcx in an application where POSE (position + orientation) estimation are required.the accelerometer and gyroscope data are written to an SD card @ 100Hz and will be post processed to keep things simple, however, if anyone has a re...

mvs1970 by Associate II
  • 2958 Views
  • 3 replies
  • 0 kudos

Problem with MS5611 Barometer Pressure Reading

Posted on November 28, 2017 at 14:27Hi all! I am trying to read temperature and pressure values (then, convert pressure to altitude) from MS5611 barometer using I2C interface with STM32F4. So far, I managed to read both temperature and pressure valu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.