2024-03-29 11:19 AM
im using the ism330dhcx in an application where POSE (position + orientation) estimation are required.
the accelerometer and gyroscope data are written to an SD card @ 100Hz and will be post processed to keep things simple, however, if anyone has a real-time algorithm that would be amazing!
2024-04-04 8:00 AM
Hi @mvs1970 ,
Have you already looked at MotionFX library?
In addition, before running the MotionFX library, I suggest you to run a calibration step with the MotionAC accelerometer calibration library, in order to minimize the residual offset of the sensor, that could sum during the integration steps.
2024-04-04 1:26 PM
@frederica,
I would very much like to use the MotionFX library, but the board I am currently using (SparkFun DataLogger IoT - 9DoF - DEV-20594 - SparkFun Electronics) already has it pre-wired to communicate using the SPI bus.
If there were an example of the MotionFX using the SPI bus, I could probably port the rest of the code, but SPI vs I2C is not an area where I have much experience or confidence.
2024-04-04 2:01 PM
Ooopppsss... just noticed that the src directory is all cortex related. This library looks great, but will be of no use to me while working w/non cortex based MCUs.
If this can be ported to vanilla arduino, then I could port it to the ESP32...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.