cancel
Showing results for 
Search instead for 
Did you mean: 

Clarification on A3G4250D Temperature Sensor Output at 25°C

shalinich67
Associate II

Dear STMicroelectronics Support Team,

I am currently working with the A3G4250D gyroscope and evaluating its temperature sensor output over I²C.

According to the datasheet, the temperature sensor output change versus temperature is specified as −1 °C per digit. I would like to clarify one point regarding the absolute digital value.

At an ambient temperature of 25°C, is there a specified or typical digital output value for the OUT_TEMP register? Or is the temperature output only defined relative to an internal reference without a guaranteed absolute value at 25°C?

In other words, should we expect a specific digital code at 25°C, or is the temperature register intended purely for relative temperature measurement and compensation?

Your clarification would help ensure correct implementation and validation during thermal chamber testing.

1 REPLY 1
Federica Bossi
ST Employee

Hi @shalinich67 ,

The A3G4250D gyroscope’s OUT_TEMP register is intended for relative temperature measurement and internal compensation only. There is no specified or typical digital output value at 25 °C, nor any guaranteed offset at room temperature. The only parameter defined in the datasheet is the sensitivity (−1 LSB/°C), which allows you to track temperature changes but not to determine the absolute temperature. No factory calibration constant or formula is provided to convert OUT_TEMP into an absolute temperature. For thermal chamber testing, you should therefore use OUT_TEMP to monitor relative temperature variation, not to validate absolute temperature.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.