2018-05-04 11:01 PM
Hello, we are building an application for condition monitoring of machines. For this, I am trying to figure out the appropriate accelerometer with the following specs: (1) a frequency response of 1.5 to 2 kHz, (2) a high ODR, higher the better, (3) an analog anti-aliasing filter, and (4) a resolution of at least 14 bits. After looking at different accelerometers, I have zeroed-in on LSM303AH and ISM330DLC (we'll be utilizing only the acc sensor). Can you please suggest which among the two should be preferred over the other (for this particular application)? Or, if these are not the appropriate ones, could you please suggest other options.
Regards,
Ankur
#accelerometer #vibration2018-05-06 5:22 AM
I would suggest to use ISM330DLC because it has 4kB and works from 1.71V to 3.6V.
The LSM303AH has only 256-lvele FIFO and works only at 1.8V.
2018-05-07 9:48 AM
Thanks Miroslav for your suggestion. Is it also possible for you to find
out what kind of anti-aliasing filter is implemented in ISM330DLC?
Best regards,
Ankur
On Sun, May 6, 2018 at 5:53 PM, Miroslav B <st-microelectronics@jiveon.com>
2018-05-09 1:31 AM
Unfortunately, this kid of information cannot be shared on the forum.
2018-05-09 3:30 PM
Sure Miroslav, I understand. Also, I was going through the data sheets of
ISM330DLC and LSM6DSL and they both seem to have mostly the exact same
specifications. Any idea what is the big/important difference(s) between
these two? Just want to ensure that we select the appropriate sensor for
our application.
Best regards,
Ankur
On Wed, May 9, 2018 at 12:02 PM, Miroslav B <st-microelectronics@jiveon.com>
2018-05-10 2:49 AM
The ISM330DLC and LSM6DSL are very similar.
The ISM330DLC is intended for industrial applications, it doesn't have Pedometer and Wrist tilt functionality. Several parameter are also guaranteed by min and max value. The ISM330DLC is part of the
http://www.st.com/content/st_com/en/support/resources/product-longevity.html
program.I think for your project the ISM330DLC is good choice.2018-05-10 3:10 AM
Thank you Miroslav!
On Thu, May 10, 2018 at 1:19 PM, Miroslav B <st-microelectronics@jiveon.com>
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.