2020-03-01 1:44 AM
Hello STM Support,
We are currently using accelerometer LIS2DH12 for the detection of following events:
Strong impact - 2.5 g or above
Free fall - 352 mg or below
Activity/Inactivity - 160 mg or above
The register settings are as follows:
Scale - 4g
CTRL1_REG - 0x37
CTRL3_REG - 0x40
CTRL4_REG - 0x88
CTRL5_REG - 0x0A
CTRL6_REG - 0x28
FIFO_CTRL_REG - 0x00
INT1_THS - 0x0B
INT1_CFG - 0x95
INT1_DUR - 0x0A
INT2_THS - 0x4E
INT2_CFG - 0x2A
INT2_DUR - 0x01
ACT_THS - 0x05
ACT_DUR - 0x20
We have a new requirement to perform step detection also. So, I was looking for sensors to achieve the above functions & step detection but I was unable to find one that can satisfy all the four requirements:
LIS2DS12 - Cannot route inactivity event to an interrupt
ISM330DHCX, LSM6DSL, LSM6DS3H, LSM6DS3, LSM6DS3TR-C, LSM6DS3H, LSM6DS0, LSM6DSR, LSM6DSM, LSM6DS33, LSM6DS3US - Cannot set different thresholds for impact detection and activity/inactivity recognition since only one register WAKE_UP_THS is available
Can you please suggest a sensor that can be used for all the four requirements? Please let me know if you need more information regarding my use case.
Thanks,
Anusha
2020-03-02 8:22 AM
Hi @AB.4 , if you have a lot (>3) of activities to be recognized from you sensor, I would suggest you to change your approach and use the finite state machine or the machine learning core features instead of the classical digital embedded features. I would suggest you to use the LSM6DSO or LSM6DSOX part numbers: up to embedded finite state machines can be programmed independently for motion detection. In the AN5273 you can find an explanation on how the FSM works, an you can find suggestions also on this Community dedicated topic flow. Regards
2020-03-02 9:01 PM
Hi Eleon,
Thanks for your suggestion. I will check it out.
Regards,
Anusha
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.