MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MEMS asm330 lhh Power-on PIN INT1 setting

Hi!I'm reading the official asm330lhh datasheet. There is a sentence "INT1 must be set to '0' or left unconnected during power-on" under Table 17 in Chapter 7. This sentence means that when MEMS is powered on, ensure that INT1 is at 0 level or Does t...

0690X00000DXQ5eQAH.jpg
CLiu.2 by Associate
  • 1761 Views
  • 2 replies
  • 0 kudos

Resolved! Sensortile.box Unable to build FP-SNS-ALLMEMS1

Hello all,I recently got the sensortile.box and was trying to play with the all mems function pack (FP-SNS-ALLMEMS1) but had trouble building the project. I have added an image of the error that I get when I try to build the project. I was able to fl...

0690X00000DXDR3QAP.png
VRao.1 by Associate III
  • 2756 Views
  • 3 replies
  • 0 kudos

Unico v9.3.0.0 missing 'ProfiMEMSToolV3.6.13.bin' file?

I downloaded the latest Unico (en.stsw-mki109w.zip) and unpacked it. Since I'm running Windows, I followed the instructions to install STM32CubeProgrammer. But when I try update the firmware, there is no .bin file in the archive. It only contains a ....

0690X00000DYOFoQAP.png
SBrow by Associate
  • 1473 Views
  • 2 replies
  • 0 kudos

Resolved! Multiple event detection on LSM6DSOX

I am developing a driver for LSM6DSOX. According to the datasheet, the module is capable of detecting free-fall, wakeup, motion detection, activity/inactivity, and so on.Is it possible, to configure multiple event detection interrupts (especially sin...

LSM303AGR Magnetometer result is deviated when iron comes nearby

Hi,we have used LSM303AGR  magnetometer for cupboard Door Open/Close detection and it is working properly.On door close position, i am getting ~0 of every direction as i have done hard iron compensation.Issue i am getting in small cupboard is to open...

APate.19 by Associate II
  • 3538 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.