2015-04-16 6:36 AM
Hi,
I'd like to knwow how I can generate a ''Write Command'', opcode = 0x52, in the Attribute Protocol.So far I'm able to send a ''Write Request'', opcode = 0x12, using the Aci_Gatt_Write_Char_Descriptor (HCI = 0xFD21).What I need now is to send a ''Write Command opcode = 0x52'' in the Attribute Protocol.I could not figure out which ACi_xxx coammnd I should be using.Could you please help me on this one ?Thank you!2015-04-16 9:55 AM
Hi PhB
Do you want to write to the attribute without a response? Do you have a speed issue? It looks like ''Aci_Gatt_Write_Without_Response'' (0xFD23) might be what you are looking for. Regards - charles2015-04-17 12:29 AM
Hello Charles,
It works now thanks to the 0xFD23 command.Thank you for your help.Reagards.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.