2015-03-27 1:51 AM
I use SPWF01SC.11to send data to server (about 6KB every 4 minutes).I split data to 2 packages (3KB each package) then send to server by TCP Socket.But sometime 1 package is lost.
Can anyone help me to solve this problem?My mail ismailto:khoatran@digisensor-co-ltd.com
</span>
Thank you.Tran Khoa.2015-03-27 2:08 AM
2015-03-27 7:42 AM
Hi,
which version are you evaluating?Can I have a full dump of configuration and status variables?Thanks, and sorry for the issue!ciaojerry2015-03-27 6:10 PM
I use firmware 141106 rel 3.3
# Dumping All Configuration Keys:# nv_manuf = ST# nv_model = SPWF01SC1# nv_serial = 1114E11454# nv_wifi_macaddr = 00:80:E1:FF:CD:56# blink_led = 0# wind_off_low = 0x00000000# wind_off_medium = 0x00000000# wind_off_high = 0x00000000# user_desc = anonymous# escape_seq = at+s.# localecho1 = 0# console1_speed = 230400# console1_hwfc = 0# console1_enabled = 1# sleep_enabled = 0# standby_enabled = 0# standby_time = 10# wifi_tx_msdu_lifetime = 0# wifi_rx_msdu_lifetime = 0# wifi_operational_mode = 0x00000011# wifi_beacon_wakeup = 1# wifi_beacon_interval = 100# wifi_listen_interval = 0# wifi_rts_threshold = 3000# wifi_ssid = 44:47:53:32:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_ssid_len = 4# wifi_channelnum = 6# wifi_opr_rate_mask = 0x00003FCF# wifi_bas_rate_mask = 0x0000000F# wifi_mode = 1# wifi_auth_type = 0# wifi_atim_window = 0# wifi_powersave = 0# wifi_tx_power = 18# wifi_rssi_thresh = 0# wifi_rssi_hyst = 0# wifi_ap_idle_timeout = 120# wifi_beacon_loss_thresh = 10# wifi_priv_mode = 2# wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00# wifi_wep_key_lens = 00:00:00:00# wifi_wep_default_key = 0# wifi_wpa_psk_raw = 84:14:B0:82:F3:D3:2E:24:06:9B:CA:BD:16:B9:9D:D0:40:10:F5:C3:AC:D7:3F:57:C2:39:D3:7D:84:D1:C9:38# wifi_wpa_psk_text = 445b926b99# ip_use_dhcp = 1# ip_use_httpd = 1# ip_mtu = 1500# ip_hostname = iwm-FF-CD-56# ip_apdomainname = captiveportal.net# ip_ipaddr = 192.168.0.50# ip_netmask = 255.255.255.0# ip_gw = 192.168.0.1# ip_dns = 192.168.0.1# ip_http_get_recv_timeout = 3000# ip_dhcp_timeout = 20# ip_sockd_timeout = 2502015-03-30 9:48 AM
Thanks for the dump.
I tried to reproduce the issue, but I had no luck. I'll keep on trying...I'll suggest you to upgrade to near coming FW3.4, when available. There are important fixes, and improved overall reliability. Stay tuned with your local ST support for FW delivery.2015-03-30 6:27 PM
Thank you,
When It is released? I waited for so long.Sory for my bad English.Tran Khoa.2015-04-01 3:06 AM
Release planned in 10 working days (after Easter period)
2015-04-02 1:52 AM
I send a buffer ex data[5]={0x01,0x02,0x03,0x00,0x04}
I use command at+s.sockw=00,5and send data[5] but module wifi only received 3 byte 0x01 0x02 0x03.It pass from byte 0x00.Is it a bug?2015-04-03 3:25 AM
Hi,
I try to figure out your use case:- Your external host sends over UART the AT-command SOCKW(5 bytes)- Module takes only 3 bytes, and never gives ''OK'' message back to external hostIs it correct?If you are not using an external host, be sure you are not sending CR and/or LF.No bug. Let me understand your use case.Regardsjerry2015-04-05 5:49 PM
{0x01,0x02,0x03,0x00,0x04}
;printf(''at+s.sockw=00,5\r'');printf(data); //Module never gives ''OK'' It's wait for 2 bytes more.printf(0x02);printf(0x03); //Module gives ''OK'' here and TCP Sever receives 0x01,0x02,0x03,0x02,0x03We’re moving the ST Community to a new platform to give you a better and more reliable community experience.