2017-10-19 11:58 AM
Hello,
I am working on a smart meter project and looking for RF transceiver IC for Sub-1GHz bands for Wireless m-bus. I found the S2-LP (
) seems to fit the requirements. Here are my question before I actually go ahead with that selection:1. S2-LP has SPI interface so I believe I can use any microcontroller with it? I am planning to use STM32L0 / L1
2. Is all the software stack available to implement wireless m-bus?
3. Do I need to use any specific compiler (like IAR) ? or I can develop using GNU ARM compiler?
4. Is there any RF module limitation i.e. do I have to use SPSGRF-868 RF module as is used in evaluation board X-NUCLEO-IDS01A4?
Any help will be very much appreciated!
thanks
Silas
#smart-metering #wm-bus #s2-lp2017-10-23 4:29 PM
Can anyone please reply? Anyone from ST please?
Thanks in advance!
Silas
2017-10-24 5:30 AM
1. S2-LP has SPI interface so I believe I can use any microcontroller with it? I am planning to use STM32L0 / L1
=> Sure. You can use any MCU. The wM-Bus example available on SPIRIT1 is based on STM32L1. You can use the same MCU.
2. Is all the software stack available to implement wireless m-bus?
=> The S2-LP library is available on web. It can be used
3. Do I need to use any specific compiler (like IAR) ? or I can develop using GNU ARM compiler?
=> X-CUBE-SUBG1 is providing example of wM-Bus in IAR, Keil, SW4STM32 (GCC) compiler. You can look at it.
The wM-Bus is provided as library
4. Is there any RF module limitation i.e. do I have to use SPSGRF-868 RF module as is used in evaluation board X-NUCLEO-IDS01A4?
=> SPSGRF-868 module is for SPIRIT1. The wM-Bus example is already available for X-NUCLEO-IDS01A4
2017-10-25 9:31 AM
Thank you so much!
Best regards
Silas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.