Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPWF04 WIND MQTT Published topic adds one character

Posted on October 23, 2017 at 10:23Hello,When I receive MQTT message it looks like one extra character is added to topic:+WIND:86:MQTT Published:0:devices/MCTEMP77/commandd:0:0:0:4:4:testTopic should be:devices/MCTEMP77/commandand not:devices/MCTEMP...

marjan by Associate
  • 964 Views
  • 1 replies
  • 0 kudos

arstechnica.com

Posted on October 17, 2017 at 08:28WPA2 Vulnerability Hello,Latest news about critical vulnerability in WPA2 has left our customers asking about the implementation in the SPWF01 modules.https://arstechnica.com/information-technology/2017/10/severe-f...

jarno2 by Associate II
  • 858 Views
  • 1 replies
  • 0 kudos

BlueNRG-MS/SPBTLE-RF Micropython drivers

Posted on December 09, 2016 at 10:23Hi Falks,i have implemented a pure python drivers (based on BlueNRG DK 2.0.2) for MicroPython.Currently i have implemented various examples:- BlueST Protocol for use 'ST BlueMS' app- SensorDemo for use 'BlueNRG' a...

SPWF01 Cant connect to AWS and AZURE

Posted on October 27, 2017 at 16:18Hello!I try to accomplish connecting and using the connection for AWS or AZURE service, but now unsuccessful. Sent: AT+S.TLSCERT2=clean,allSent: AT+S.SETTIME=1509036785OKOKSent: AT+S.SETTIMEOK# Date and GMT Time:# ...

Firmware update

Posted on October 10, 2017 at 15:58Hello all,I would like to udpate the firmware on the BLE, I am using an external processor and BLUENRG-1, both of them are connected by SPI and UART but I will be using SPI. I would like to update the firmware, I h...

jampino by Associate III
  • 3684 Views
  • 13 replies
  • 0 kudos

Write unique ID

Posted on August 16, 2017 at 16:58Hello everyone,I have the BLUENRG-1 running and working ( advertising, creating connections, sleeping ).Now I would like to write a unique ID in each bluenrg-1 and then read it when the application starts up but not...

jampino by Associate III
  • 801 Views
  • 3 replies
  • 0 kudos

How to tell when BlueNRG is transmitting?

Posted on October 25, 2017 at 03:34I'm working on a product where the BlueNRG RF during transmit is affecting our measurements.  I was wondering if the TEST8 or TEST9 pins would be useful in avoiding the periods when BlueNRG is transmitting?  I noti...

rdscliff by Associate II
  • 620 Views
  • 0 replies
  • 0 kudos

SPWF04 SPI Socket Server Problem

Posted on October 24, 2017 at 13:06SPWF04 SPI SOCKET SERVERI have the SPWF04SA configured as an STA and connected to a Wifi AT.I have an udp  socket server opened in the SPWF04, for that I have used the following sentence:                AT+S.SOCKDO...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.